I got my module today. I can’t solder wires to the SMT connector. So I am going to solder wires directly to the board.
I also just posted this note to the comments section for the module:
jsampson:
I have found a discrepancy in the data sheets.The data sheet from SPK says “BATTERY input range 1.6V ~ 5.1V.” The data sheet from u-blox says that maximum ratings are “Backup battery voltage,(V_BCKP) Vbckp, min=-0.5 max=3.6”.
So it looks like applying higher than about 3.3V may blow out the battery backup input. I don’t see a regulator on the board for this. There does appear to be a series diode on the board.
I am planning to use a 3V lithium battery.
I’ll post more as I make progress.