Need 5 PWM outputs from a single timer

I’m working on an Uno R3 based controller for 5 channels of LED strip lighting. The problem is that there is a subtle flicker when all channels are powered. The flicker is caused because the default PWM outputs are run at different frequencies. Timer 0 (pins 5 & 6) runs at 976.5625 Hz, Timer 1 (pins 9 & 10) at 490.20 Hz, and Timer 2 (pins 11 & 3) at 490.30 Hz. Timer 0 is almost, but not quite, 2X the frequency of Timer 1 & 2. This is causing a beat frequency that results in the flicker. Does the Arduino Pro use the same 3 timer configuration to control the PWM output? Do any versions of Arduino, besides the Mega, have at least 5 PWM outputs that run at the same frequency?

Have you tried changing the frequency to something faster?

http://playground.arduino.cc/Code/PwmFrequency

Nope, I’ve just been using the default frequencies. I’ll do some tests with higher frequencies.