Need a part#

Anyone have a part number for a shrouded 6 pin header (for use on target) to mate with the 6 pin ISP connector? I am not sure which brand of connector is used on the programmer (AVRISP MKII). I see that Sparkfun has a header for the 10 pin, but not the 6 pin.

Thanks,

Jamie

What I’ve done in the past is used a plain 0.100" male headers (typically solder in two rows of single row break-away headers [like these). All you need to do is make visible indicator for pin 1. (e.g. silkscreen label)

Otherwise you could buy the Molex brand shrouded header [90130-1106 dual row, 6-pins.](Break Away Headers - Straight - PRT-00116 - SparkFun Electronics)](Break Away Headers - Straight - PRT-00116 - SparkFun Electronics)