I have a Siemens TC35 GSM board i need to wire up to a Arduino Uno compatible board (See Picture Below). Do i have to use the RS232 connector to access it or can i do it thru the jumper wires or terminals. It would be nice if someone could post a pictorial wiring diagram or photo. The Arduino Board is a Salid Arduino Uno board with built in GPS.
Any help would be great
Thanks a bunch
George
 https://sites.google.com/a/datapointcom … 7small.jpg
https://sites.google.com/a/datapointcom … 7small.jpg
High Res Photo of Both Boards
http://dl.dropbox.com/u/6339586/both.jpg
High Res Photo of GSM Board
http://dl.dropbox.com/u/6339586/gsm.jpg
High Res Photo of the Arduino + GPS Board
http://dl.dropbox.com/u/6339586/arduino.jpg
GPS Manual
http://www.cutedigi.com/pub/GPS/SR-92_U … ual_EN.pdf\
Arduino with GPS Schematic
http://dl.dropbox.com/u/6339586/gps%20schematic.pdf
GSM Schematic
http://www.yourportablelab.com/download … CH+PCB.pdf
TC35 Manual (GSM)