Need help with my project

Hello, I am a newbie to ardunio. I built an alarm system using PIR sensor, LED bulb, Ardunio Uno and Adafruit CC3000 Wifi Shield and now i am having some problems. I have also built an android mobile application to this project

First the LED bulb lights up slightly when motion is detected.

I have created a code which send notifications to my android application when motion is detected. but i dont receive notifications when the pir sensor detects motion. but the android application receives a notification when i upload the code to the Ardunio Uno board. I have no idea where the problem is or how to correct it.

#include <Adafruit_CC3000.h>
#include <ccspi.h>
#include <SPI.h>
#include <string.h>
#include "utility/debug.h"

// These are the interrupt and control pins
#define ADAFRUIT_CC3000_IRQ   3  // MUST be an interrupt pin!
// These can be any two pins
#define ADAFRUIT_CC3000_VBAT  5
#define ADAFRUIT_CC3000_CS    10
// Use hardware SPI for the remaining pins
// On an UNO, SCK = 13, MISO = 12, and MOSI = 11
Adafruit_CC3000 cc3000 = Adafruit_CC3000(ADAFRUIT_CC3000_CS, ADAFRUIT_CC3000_IRQ, ADAFRUIT_CC3000_VBAT,
                                         SPI_CLOCK_DIVIDER); // you can change this clock speed

#define WLAN_SSID      "dlink_DWR-730_1A31"            // cannot be longer than 32 characters!
#define WLAN_PASS       "hAMpU34443"
// Security can be WLAN_SEC_UNSEC, WLAN_SEC_WEP, WLAN_SEC_WPA or WLAN_SEC_WPA2
#define WLAN_SECURITY   WLAN_SEC_WPA2

#define IDLE_TIMEOUT_MS  3000      // Amount of time to wait (in milliseconds) with no data 
                                   // received before closing the connection.  If you know the server
                                   // you're accessing is quick to respond, you can reduce this value.

// What page to grab!
#define WEBSITE      "www.m-register.com"
#define WEBPAGE      "/urlval.php?status=true"
int sensor=7;
int push_switch=2;
int buzzer=8;
int sensor_value;



uint32_t ip;

void setup(void)
{
  Serial.begin(9600);
  Serial.println(F("Hello, CC3000!\n")); 

  Serial.print("Free RAM: "); Serial.println(getFreeRam(), DEC);
  
  /* Initialise the module */
  Serial.println(F("\nInitializing..."));
  if (!cc3000.begin())
  {
    Serial.println(F("Couldn't begin()! Check your wiring?"));
    while(1);
  }
  
  // Optional SSID scan
  // listSSIDResults();
  
  Serial.print(F("\nAttempting to connect to ")); Serial.println(WLAN_SSID);
  if (!cc3000.connectToAP(WLAN_SSID, WLAN_PASS, WLAN_SECURITY)) {
    Serial.println(F("Failed!"));
    while(1);
  }
   
  Serial.println(F("Connected!"));
  
  /* Wait for DHCP to complete */
  Serial.println(F("Request DHCP"));
  while (!cc3000.checkDHCP())
  {
    delay(100); // ToDo: Insert a DHCP timeout!
  }  

  /* Display the IP address DNS, Gateway, etc. */  
  while (! displayConnectionDetails()) {
    delay(1000);
  }

  ip = 0;
  // Try looking up the website's IP address
  Serial.print(WEBSITE); Serial.print(F(" -> "));
  while (ip == 0) {
    if (! cc3000.getHostByName(WEBSITE, &ip)) {
      Serial.println(F("Couldn't resolve!"));
    }
    delay(500);
  }

  cc3000.printIPdotsRev(ip);
  
  // Optional: Do a ping test on the website
  /*
  Serial.print(F("\n\rPinging ")); cc3000.printIPdotsRev(ip); Serial.print("...");  
  replies = cc3000.ping(ip, 5);
  Serial.print(replies); Serial.println(F(" replies"));
  */  

  /* Try connecting to the website.
     Note: HTTP/1.1 protocol is used to keep the server from closing the connection before all data is read.
  */
  Adafruit_CC3000_Client www = cc3000.connectTCP(ip, 80);
  if (www.connected()) {
   www.fastrprint(F("GET "));
    www.fastrprint(WEBPAGE);
    www.fastrprint(F(" HTTP/1.1\r\n"));
    www.fastrprint(F("Host: ")); www.fastrprint(WEBSITE);www.fastrprint(F("\r\n"));
    www.fastrprint(F("\r\n"));
   www.println();
  } else {
    Serial.println(F("Connection failed"));    
    return;
  }

  Serial.println(F("-------------------------------------"));
  
  /* Read data until either the connection is closed, or the idle timeout is reached. */ 
  unsigned long lastRead = millis();
  while (www.connected() && (millis() - lastRead < IDLE_TIMEOUT_MS)) {
    while (www.available()) {
      char c = www.read();
      Serial.print(c);
      lastRead = millis();
    }
  }
 www.close();
  Serial.println(F("-------------------------------------"));
  
  /* You need to make sure to clean up after yourself or the CC3000 can freak out */
  /* the next time your try to connect ... */
  Serial.println(F("\n\nDisconnecting"));
  cc3000.disconnect();
  
}

void loop(void)
{ sensor_value=digitalRead(sensor);
  //Serial.println(sensor_value);
  if(sensor_value==HIGH)
  {
    digitalWrite(buzzer,HIGH);
  }
  if(digitalRead(push_switch==HIGH))
  {
    digitalWrite(buzzer,LOW);
  }
 delay(1000);
}

/**************************************************************************/
/*!
    @brief  Begins an SSID scan and prints out all the visible networks
*/
/**************************************************************************/

void listSSIDResults(void)
{
  uint32_t index;
  uint8_t valid, rssi, sec;
  char ssidname[33]; 

  if (!cc3000.startSSIDscan(&index)) {
    Serial.println(F("SSID scan failed!"));
    return;
  }

  Serial.print(F("Networks found: ")); Serial.println(index);
  Serial.println(F("================================================"));

  while (index) {
    index--;

    valid = cc3000.getNextSSID(&rssi, &sec, ssidname);
    
    Serial.print(F("SSID Name    : ")); Serial.print(ssidname);
    Serial.println();
    Serial.print(F("RSSI         : "));
    Serial.println(rssi);
    Serial.print(F("Security Mode: "));
    Serial.println(sec);
    Serial.println();
  }
  Serial.println(F("================================================"));

  cc3000.stopSSIDscan();
}

/**************************************************************************/
/*!
    @brief  Tries to read the IP address and other connection details
*/
/**************************************************************************/
bool displayConnectionDetails(void)
{
  uint32_t ipAddress, netmask, gateway, dhcpserv, dnsserv;
  
  if(!cc3000.getIPAddress(&ipAddress, &netmask, &gateway, &dhcpserv, &dnsserv))
  {
    Serial.println(F("Unable to retrieve the IP Address!\r\n"));
    return false;
  }
  else
  {
    Serial.print(F("\nIP Addr: ")); cc3000.printIPdotsRev(ipAddress);
    Serial.print(F("\nNetmask: ")); cc3000.printIPdotsRev(netmask);
    Serial.print(F("\nGateway: ")); cc3000.printIPdotsRev(gateway);
    Serial.print(F("\nDHCPsrv: ")); cc3000.printIPdotsRev(dhcpserv);
    Serial.print(F("\nDNSserv: ")); cc3000.printIPdotsRev(dnsserv);
    Serial.println();
    return true;
  }}

I have used the Webclient example in the ardunio.I need to build my code such that it send a true message to the given website when the sensor detects motion.

I dont know how to edit this code. What should i Do?

Yuuki