Need help with TX based on rfm-ro2100 resonator /or?

Hello all! I have a supply of TX’s and RX’s that I would like to use. Problem is that the TX use a RFM-R02100 resonator and I don’t know how to use it with my AVR. I have read the schematic and there is a low power TX application, but I am not knowlegable enough to know what values to use and how to feed a modulation input to make a 295.05 MHZ TX’r. Can anyone please suggest some ideas on how I can get my hands on a 295.05 MHZ TX’r that is IC based, or if someone can help me modify my existing TX’r which currently has a PIC in it but I would like to use an AVR instead. Please help as I have more than a few of these ready made TX’s and RX’s which are well designed but I cannot use them without being able to use the transmitter. Thank You, Lupe.