Hi There ![]()
I’M new to this this web-site. And I’M have a problem.I’M trying to Interface the CYWM6935 WirelessUSB LR Radio/Module to the Arduino Duemilanove And I’M not sure how to wire it up? I need the pin/out ? On the CYWM6935 There is A 12 Pin Header Connector on the module. pin1 -GND… pin 2-VCC …pin3-IRQ… pin4-nRESET… pin5-MOSI… pin6-MISO… pin7-SCK… pin8-MISO… pin9-GND… pin10-nPD…
pin11-N/C… pin12-N/C. No problem with the two gnds and the 3.3volt VCC line.but what pin goes to the IRQ-3 & nRESET-4&MOSI-5&nSS-6&SCK-7&MISO-8&nPD-10 From the Arduino Duemilanove bd.
Thanks:Allan :?: