New Color LCD ARM software released

Ok boys, have at it. I revised much of my original code and ported it over to the ARM platform. Nathan was kind enough to put it up on the Color LCD site today (thanks Nathan!)

I must say, using the ARM to drive the Color LCD is awesome! Its now super fast to display images. I have added a routine to enable the 4096 color mode. fixed the circle routines for better performance, and done some other performance changes. there is a full demo there for the CrossWorks development package. For those of you with the "Development Board Atmel SAM7 ARM " and this Color LCD, down load the code, and connect the LCD to the header. the connections are as follows:

Board Connections

Olimex ARM Board header (the long strip) — LCD carrier Board

3.3V – Vin

PA11 – ~CS

PA13 – SDATA

PA14 – SCLK

PA15 – RST

GND – GND

Thats it!

then flash the ARM to watch the demo, its cool.

I also took a video of it and is posed here.

http://digitalimagination.us/sparkfun/SparkFun.wmv

and now onto my 2.2" touch screen i bought!!! YA-HOOO…