I purchased two kits a RTK Express and RTK Surveyor. I cannot get the RTK Express to charge. I can connect via the usb connectors on the unit but when I plug it in to the include charger and cable it will not charge. I have used multiple cables, charging bricks and cooled the unit off (read thermal issues with battery) and nothing will work.
Help.
             
            
              
              
              
            
            
           
          
            
            
              The battery connector may have become disconnected; if you are comfortable you may open the unit up and ensure the battery cable is plugged in https://docs.sparkfun.com/SparkFun_RTK_ … /#surveyor
Any luck?
             
            
              
              
              
            
            
           
          
            
            
              Checked the connection. It is fine. there seems to be an issue from the usb slots to the battery. Running 3.7 and 1.32 firmware. Would like to send it back. Thank You
             
            
              
              
              
            
            
           
          
            
            
              If purchased from us head over to www.sparkfun.com/returns and we’ll get ya squared away; contact vendor if purchased elsewhere