I want to use copper tape to connect two pennies to a 3v coin battery and an let light. Then each of the two kids touches a penny and they touch each other, thus closing the circuit and lighting the bulb. All of this would be in a simple valentines card. Does this sound workable?
Yes. I’ve seen similar LED lights done w/a coin cell, an LED and thin wires. The resistance of the wires and the internal resistance of the coin cell were enough to limit the current through the LED … so that it wouldn’t burn out.
The problem I forsee is the connection between coppertape and the pennies. Is there a conductive path between them or is the sticky side of the tape (or whatever used to fix them together) perhaps isolating?
0987:
I want to use copper tape to connect two pennies to a 3v coin battery and an let light. Then each of the two kids touches a penny and they touch each other, thus closing the circuit and lighting the bulb. All of this would be in a simple valentines card. Does this sound workable?
The idea could work very nicely but you or someone will need to construct a circuit for it to work effectively. Use one of those quarter size flat 3 volt batteries. It is only ON when the pennies are touched, no need for a switch.
I did a little experiment just now. Using 3 volts directly with a LED that had a 1.2 forward voltage, it would not light up with the pennies placed on both sides of my tongue which was the most conductive part of myself available. :o
With spit on my fingertips on opposite hands my body resistance is 500K.
The 1.2v LED @ 3v only showed useful brightness if the resistance was less than 3000 ohms while 1000 ohms was ideal.
The Darlington pair drops about 1 volt while the LED drops ~1.2 volts. That leaves ~.8v / 100R = 8 ma through the LED. R1 protects against the pennies being touched together.
It is important to use an LED with the lowest forward voltage rating, 1.2 volts is ideal.