Hi!
Just got my Bluegiga WT32 Breakout board in the mail today, hooked it up to my computer to configure it.
But I cannot get any reply from it…
It’s connected from my Com port to a MAX3225 converter, and then to the WT32 unit.
If I short tx/rx on the WT32 side, and I get an echo back on my RealTerm window.
This is how I have wired up my WT32:
-
GND and RESET - GND on my breadboard, MAX3225 and com
-
Vcc and BTEN - 3.3v
-
TX0 - (T1IN - T1OUT) - RXD
-
RX1 - (R1OUT - R1IN) - TXD
Any suggestions would be highly appritiated ![]()
Edit:
I downloaded the “BGTerm” from blugegiga.com, only reply I’m getting from the device is “\xff” which i guess from the google reply’s is not comming from the device at all, but is some terminal stuff from my computer?
Looks like this was a 100 bucks out the window…