Hi all, I’m new to this forum and already find it quite helpful,
I’m trying to use the Nordic’s rf2401, and I started to do so by following
the demo for ShockBurst link that is on the Configurator User Guide.
I’d hate to say this but I can’t seem to be able to receive anything !
I’ve checked that the data, CE(chip enable) and clock signals are going into the evaluation board, but as I don’t have a spectrum analyser, I can’t check if the signals are sent out from the antenna.
I’m using two serial ports on one computer, and also have tried
two computers with a configurator+evaluation board on each.
I’m using the SW provided by Nordic as well (called nRF configurator).
You could see that I’ve done everything that the user guied tells me to do.
Could noise be an issue? Do the antenna have to be in line of sight ?
Did anyone else have similar problem ?
Or can anyone direct me to where I should look for problem ?
Cheers -