First up - thanks for the tutorials, which have been really handy so far. I have a remaining problem with getting Dynamic Payload Widths to work, which is pretty much the last thing I need to understand.
I have two NRF24L01 modules, attatched to individual MCU’s. Basic to and fro works fine, I’ve switched to DPL because I am wanting to send packets in excess of 32 bytes between the two, and don’t want to have to send in multiples of 32 bytes all the time.
On the TX side, my send routine cuts the packet into <32 byte chunks and sends them individually (sends the first, waits for an interrupt meaning it sent successfully or timed out waiting for an ack, then sends the second.) I can see that on a 36 byte packet the first 32 bytes send OK, and the remainder time out waiting for an ack. Maybe not the fastest way, but speed isn’t that critical.
On the RX side, bizarre stuff is going on! I receive the RX_DR interrupt, and drop CE. I then try and issue R_RX_PL_WID to read the payload width. This returns me 0x40, which is clearly wrong. I do R_RX_PAYLOAD which I cap at 32 bytes - if I try and read more I get gibberish as you’d expect. I then raise CE, but don’t get any more data.
Things I am not doing…
-
RX_FLUSH: tried this in various places to no effect.
-
Reading payload length AFTER reading the data - all this did was give me the return value of 0x4E instead of 0x40
I’d really appreciate some help on this as I’m struggling to see how this all fits together and up till now it’s been reasonably sane. ![]()