I have the nRF24L01+, one with the antenna
i use two arduino uno
i am read all the possible post and cannot get them to communicate
i have added a capacitor on the power input
i have used the getting started example and the status message shows that it is setup correctly
when i set one of them as T it looks as if it is communicating even if i power down the receiver
when i do the same on the other unit i get a failed message
the tx LED does not blink although the rx does.
i have spent days without success and hope that someone has the answers
thanks