Hi all,
I’ve been “experimenting” with NRF24L01+ and 2xLPC1343 for some time, and I came across two things I cannot figure out on myself.
- I cannot switch between RX and TX mode.
If I set RX and then sets TX and tries to send a packet,nothing happens. If I restart the module,set to TX and send, its OK. If its at RX, it receives
- When the receiver is not ON, the module “hammers” the uC with interrupts instead of issuing 1 interrupt for max retries. I watched it with oscilloscope, the NRD24L01+ issues interrupt every ~1ms and when read it back, the MAX_RT flag is on. You can check the code below, but I think I clear the interrupts properly + flushing the TX + clearing CE bit, but still the module becomes un-usable after I try to send a packet with the receiver OFF. I have to restart the whole board in order to get it up&running again.
I am using 2 LPC1343 boards ( one olimex’ and one self made ) with different pin assignment, but the same NRF code - i.e. the NRF part is the same on both boards.
If TX module is ON and the RX is ON ( both configured ) the transmission is OK. If I change the RX/TX side, its again all OK.
I assume its the software, because it does not matter which board tries 1) or 2), its always the same.
The code I use is
void nrf24_init(unsigned char freq, unsigned char power, unsigned char rate, unsigned char lna_gain) {
if(( freq > 125 ) && ( freq < 0 )) {
NRF_FREQ = 0;
}
else {
NRF_FREQ = freq;
}
NRF_RFSETUP = power | rate | lna_gain ;
nrf_wr_reg(NRF_WRITE_REG + NRF_EN_AA, 0x1);
nrf_wr_reg(NRF_WRITE_REG + NRF_EN_RXADDR, 0x01);
nrf_wr_reg(NRF_WRITE_REG + NRF_SETUP_RETR, 0x0);
nrf_wr_reg(NRF_WRITE_REG + NRF_RF_CH,NRF_FREQ);
nrf_wr_reg(NRF_WRITE_REG + NRF_RF_SETUP, NRF_RFSETUP);
nrf_wr_buf(NRF_WRITE_REG + NRF_RX_ADDR_P0, (unsigned char*)RX_ADDRESS, NRF_ADR_WIDTH);
nrf_wr_reg(NRF_WRITE_REG + NRF_RX_PW_P0, NRF_RX_PLOAD_WIDTH);
nrf_wr_buf(NRF_WRITE_REG + NRF_TX_ADDR, (unsigned char*)TX_ADDRESS, NRF_ADR_WIDTH);
nrf_wr_reg(NRF_WRITE_REG + NRF_STATUS, NRF_CLRST);
}
void nrf_rx_mode(void) {
nrf_ce(NRF_CE_DESEL);
nrf_wr_reg(NRF_WRITE_REG + NRF_CONFIG, 0x03);
delay(1000);
nrf_ce(NRF_CE_SEL);
}
void nrf_tx_mode(void) {
//nrf_ce(NRF_CE_DESEL);
nrf_wr_reg(NRF_WRITE_REG + NRF_CONFIG, 0x02);
delay(1000);
//nrf_ce(NRF_CE_SEL);
}
void nrf_flush_tx (void ){
nrf_wr_reg(NRF_FLUSH_TX,0x0);
}
void nrf_txpacket(unsigned char *tx_buf) {
nrf_wr_buf(NRF_WR_TX_PLOAD, (unsigned char*)tx_buf, NRF_TX_PLOAD_WIDTH);
}
void main (void)
...
case '<transmit>' :
txrx_mode = 0x1;
nrf_tx_mode();
send_msg("NRF:Set to TX mode");
break;
case '<receive>' :
txrx_mode = 0x0;
nrf_rx_mode();
send_msg("NRF:Set to RX mode");
break;
case '<send_pkt>' :
if (txrx_mode) {
nrf_txpacket((unsigned char*)nrftxbuf);
nrf_ce(NRF_CE_SEL);
delay(1000);
nrf_ce(NRF_CE_DESEL);
} else {
send_msg("NRF:Cannot execute while TX not configured");
}
then interrupt procedure
if (nrf_interrupted) {
if (txrx_mode) {
nrf_status = nrf_rd_reg(NRF_STATUS);
if (nrf_status & NRF_TXDS) {
send_msg("NRF send successful");
} else if (nrf_status & NRF_MAXRT) {
nrf_ce(NRF_CE_DESEL);
send_msg("NRF not sent - MAX Retries reached!");
} else {
nrf_flush_tx();
nrf_ce(NRF_CE_DESEL);
bytetohex(nrf_status);
send_msg("NRF not sent");
}
nrf_wr_reg(NRF_WRITE_REG + NRF_STATUS, nrf_status);
} else {
if (nrf_rxpacket((unsigned char *)nrfrxbuf)) {
delay(10000);
send_msg("NRF received successful");
} else {
send_msg("NRF received NOT successful");
}
}
nrf_interrupted = 0x0;
the wr_reg and rd_reg are “verified” separately and the tasks are working - I don’t think the issue is there. I have tried different register write and read-back, the “checks” are OK.
If someone has an idea for help, please comment, as I am not able to figure out where the problem is…
Thanks in advance ![]()