nrf24L01 receiving problem

I designed an application where a nrf24L01 is driven by an arm7.

no problem for configuration of the module and transmit data, but i can’t receive anything (ACK or data)

i verified the emitter by sending data to a nordic module which receive it : but i don’t receive ACK

transmitter and receiver configuration are exactly the same :

RQDIOConfigure(); //config = 0x09

RADIODisable(); // CE LOW

RADIOCloseAllPipe(); // First close all radio pipes

// Pipe 0 and 1 open by default

RADIOCRC16Set(); // Operates in 16bits CRC mode

RADIOAutoRetransmitConfigure();

RADIOAddressWidthSet();

RADIOTXADDRSet (address);

RADIOP0ADDRSet (address);

RADIOP1ADDRSet (address2);

RADIOP0Enable();

RADIOP1Enable();

RADIOPXAASet();//enable aa for pipe 0 and 1

if( mode == TXMODE) // Mode depentant settings

{

RADIODriverTXMode();

}

else

{

RADIODriverRXMode();

RADIODriverPayloadWidthSet( PAYLOAD_LENGTH);

}

RADIODriverChannelSet(RF_CHANNEL);

RADIODriverPWRUPSet(); // pwr up bit and wait 5ms

for emitter sofware i use :

while (1)

{

wait(500);//500ms

RADIOStatusClear();

RADIOPayloadWrite(message);

RADIOCEPulse(); // generate a >10us pulse

}

for receiver software i use :

while(1)

{

RADIOEnable(); // CE HIGH

// read status regsiter and compare RX_DR

do{

RADIODriverRegisterRead(R_STATUS, &data, 1);

}

while( (data & 0x40)==0);

}

= data always equal to 0x0E

Any idea ?