nRF24L01 temperature

Just to tell you I succed to transmit data (3 bytes, 2MBPS @100Hz) at 125°C in a climatic chamber. The PRX was inside the chamber and the PTX outside.

I used WRL-00691 module.

Hi,

can you tell me what values you programmed in to the nRF24L01 registers?

for the receiver and the transmitter.

Thanks in advance.

I wrote the same value as you in your previous post.

so, you used our value’s? and it worked correctly? also the same transmit way?

if thats so it only can be a hardware problem :?

fignon:
Just to tell you I succed to transmit data (3 bytes, 2MBPS @100Hz) at 125°C in a climatic chamber. The PRX was inside the chamber and the PTX outside.

I used WRL-00691 module.

**Thankyou** very much for sharing this!!

I have an future project that will use a nRF24L01+ in high temp environments (100-125 degrees Celsius).