Hi,
I just bought 2 nrf9160 Thing Plus boards. I registered the SIMs at hologram.io.
I connected the first device and it came up with a pulsing blue LED and the serial port was printing these msgs:
[00:02:06.661,163] <inf> app: Accel reading: #126 @ 126661 ms
It responded to typing AT with an OK.
Problem #1: I tried to connect to the nordic LTE Link Monitor and it couldn’t find any serial ports. This is on a Mac and seem to have the driver since Cool Terminal seems to be able to see the port.
–Shouldn’t it show up?
I manually entered AT+CFUN=1 and after some time I saw that it connected to T-Mobile on the hologram dashboard.
Problem #2: I connected the second board (w/SIM) and there was no blue pulsing LED and no output on the serial port.
–Is this board dead?
– Was it not pre-programmed with something?
I am still trying to plow through building code for it and flashing it, but I’d like to know if there is a problem with the board. Is there something I can easily try to program onto the board? Holding down the mode button while resetting doesn’t seem to cause any different behavior.
Thanks!