Hello community,
I am very new in the arduino scene, this is probably the reason why I do not understand how to communicate with the wifly shield!
of course there is a tutorial which combines the speakjet unit, but for some reason I feel lost by reading it because as I said, I’m a newbie.
Can please someone help me how to communicate with my wifly shield? I think someone just need to show me the right direction how to do that
Thanks in advance!
By the way, all I can say is the green led is blinking slow, the orange one fast, and the red one is blink very very slow I also use arduino uno and I am not sure if I soldered wiflyshield right
Edit: It seems like at least I get the message “Bridge initialized successfully!”, that’s good!
Another edit: Didn’t know that I am able to read the Serial prints…
WiFly Shield Terminal Routine
Bridge initialized successfully!
Rebooting
Entering command mode.
Set wlan to authorization level 3
Set security phrase to 1881******
Set IP localport to 8
Joining 'arigato'
WG÷·77÷·Ø@Failed to associate with 'arigato'
Retrying...
Rebooting
Entering command mode.
Set wlan to authorization level 3
Set security phrase to 1881******
Set IP localport to 8
Joining 'arigato'
...
Edit edit:
I made an image to visualize which information I wrote down into the wifly autoconnect script:
http://img209.imageshack.us/img209/9924/fritzbox.png
Edit edit edit: After reading lots of stuff, I found out that I can scan, how do print out what wifly scanned for networks? Something like…
String donkey = SPI_Uart_print("scan");
Serial.println(donkey);
?
Regards again
Soelen