Oled 3V AVR 5V

Has anyone used this OLED with an AVR? http://www.sparkfun.com/commerce/produc … cts_id=712

Looking at the data sheet it says

Logic Supply 2.4-3.5v

High Logic Input Min 0.8*VDDIO

Low Logic Input Max 0.2*VDDIO

That makes the low for 0.66 if I run the screen at 3.3v. Do you think the diode method will work for this?

EDIT: I have diodes 1N5818 and the data sheet says max forward voltage (I<=100ms) is 330mv. When I tested it with my multimeter it read 0.123V. These will work correct?

Thanks,

Justin