Hi , I’m the lucky owner of an OLIMEX board based on the AT91SAM9260 .
In the NAND flash there’s already installed the linux kernel and I can connect to it via an rs232 cable with my laptop equipped with LINUX UBUNTU 8.04.
I’ve a question about the ethernet connection with wich I can connect to the board to transfer files between the host laptop and the ARM target board .
Do I need an ethernet hub and two ethernet cable or can I simply use a twisted ethernet cable?
Thank you very much.