Can anyone tell me if Olimex made a mistake not setting it up the CD for LPC-2103?
Do I have to modify anything or will the blink LED 2148 project work for a 2103?
I am progressing but I have got the following when I do the Debug:
(gdb) target state: halted
target halted in ARM state due to debug request, current mode: Abort
cpsr: 0x600000d7 pc: 0x000002f4
flash ‘lpc2000’ found at 0x00000000
erased sectors 0 through 0 on flash bank 0 in 0s 500560us
wrote file main.bin to flash bank 0 at offset 0x00000000 in 0s 297208us
requesting target halt and executing a soft reset
force hardware breakpoints enabled
then I pressed resume and got
in the Disassembly window.Target request failed: putpkt: write failed: Connection reset by peer…
Any help much appreciated.