Olimex LPC-H2888

Just wondering if anyone knows of the status of the Olimex LPC-H2888.

The Olimex website indicates that this board will be available Oct 2006.

I am very keen in getting one of these boards. Any information on availability and pricing would be greatly appreciated.

I asked Olimex last week, and they told me it’ll be available by the end of october. The price is $100/each.

A bit expensive IMHO, but still a very interesting board indeed.

Are you kidding? It has plenty of memory and flash for uCLinux. If it is $100 I’m definitely getting one. Unless the EP9315 board is under $160, then I’ll get that one.

Am I the only one wishing the LPC2888 had an MMU? With the LCD controller and SDRAM controller already in there, the MMU is the only thing missing for Windows CE, PalmOS etc. Cant wait for LPC3180

I’m also waiting on the Olimex LPC-H2888.

I want one bad too, but $100 bucks seems a bit steep for that board.

so we are way past the release date, whats the deal Olimex ?

Interested as well. Olimex’s website is now saying

PRELIMINARY INFO, THIS BOARD WILL BE AVAILABLE FOR SALE APRIL-MAY 2007

. I emailed info@olimex.com about a week ago to ask if this date was still valid, and haven’t heard back.

Hope it’s released soon!

ya, i never have gotten a response from them when asking about release dates. I think they got to many sticks in the fire, then should work on what they can handle instead of promising a bunch of stuff and then don’t deliver.

Hey Olimex, when is this bad boy gonna be released ???

I’ve sent two emails, both went unanswered. The site says April-May. Well, today is the last day of May.

I could really use this!!

i could use it as well. I just hope they dont over price it when it does come out.

Still, price is not much of an issue for me. There’s really nothing decent out there right now with Hi-Speed USB, at least not that I could find that’s going to be priced anywhere near this. So I guess price is an issue, I just don’t think, whatever they decide, that it’ll be anywhere near as high as the competition for Hi-Speed USB Dev Boards.

i agree, but dont let them know that we dont care what the cost is :smiley:

Price would be an issue for me.

I’m waiting on 3 parts from Olimex… LPC2888, the 9315 and LPC-L2294-8MB. I’ve been designing my own LPC-L2294-8MB board lately, maybe I’ll build it before Olimex (my sram (Cypress) parts are more readily available than the Samsung PSRAMs that are holding Olimex back, albeit at a higher cost). I’m also hoping to use the expensive MRAMs instead of the flash. MRAMs kick butt for prototyping because they’re fast and writes are not limited.

What’s holding ME back is the fact that the Eagle library is limited on footprints and I’m learning how to make footprints.

OK Olimex, I know you watch these forums. So listen closely!!!

I don’t know how things are done over there in BULGARIA, but over here in the good old U.S.A. its considered RUDE when someone asks you a question and you don’t even take the time to reply.

Let alone, to have several people ask, and yet you still give no reply. Get it together and let us know once and for all what is the story with this LPC-H2888 release date ?

I think we are all old enough to handle the truth of the matter.

***
PRELIMINARY INFO, THIS BOARD WILL BE AVAILABLE FOR SALE APRIL-MAY 2007
***

ya, i get it, but this date usually changes every month or so.

so quite teasing.

Hi,

Somehow I missed this tread, so I’ll clarify the situation with LPC2888 and I hope you will understand.

LPC2888 is the most complex board we have made as technological challenge and as complexity and as incomplete documentation we ever dealt so far. I also appreciate all the help we got from NXP gurus and I confess that without their excellent support we would never be able to finish this board (we were in correspondence with over 6 NXP engineers from California to China who provide us with all documents available in NXP about this project).

The development work started in June 2006 and was sucessfully finished May 2007 so we worked on this board 11 months, yes there were anoncements on our web that it will be released September 2006 then October 2006 then March - April 2007 I guess we have been too optimistic :slight_smile:

I appreciate the patience all you had and the number of e-mails showing interest for this board.

The truth is that we had to go through dozen of PCB prototypes and revisions of the board caused by number of reasons.

The only alternative board for this chip is from Nohau and those who have spent $1200 have probably found later that on Nohau boards the SDRAM is working only up to 30 Mhz , on our final prototype we made the SDRAM works on the maximum LPC2888 frequency 60 MHz without problems.

There are not well known problems with the on chip DC/DC converter which works on 1 Mhz and cause lot of torubles to other parts in the MCU including some side effects like if you run the LPC2888 once on internal DC/DC with 1.5V single cell source it burns something inside the chip and you can’t use external power supply anymore but only the internal 1.5V DCDC.

For those who are familiar with the Nohau schematic just ask yourself why Nohau placed 2 external DC/DC convertors when the chip have internal DCDC? But to be objective I will confess that Nohau board works well with the both internal and external DCDC converters, so obviously the internal DCDC may be used correctly with properly routed board.

On our latest prototype this DCDC again behaved weird, but we just decide to make one final attempt to route it differenlty (note that even if you change track routing with 1 cm it gives totaslly different picture on the scope), so if it will not work as needed on this final revision of the board we’ll just disable it and tell anybody to not use it with our board unless he wants to power the boards with only 1.5V :slight_smile:

So the blank boards will be ready in days and we start the assembly. I’ll keep you in touch and crossing my fingers to have sucess with the DCDC so to have everything working on the final release.

Best regards

Tsvetan

Now that is what i call a great reply.

you should have just said that from the beginning, we would have all understood.

Thanks and keep us posted.

It is true that sometimes it takes time to get an answer from Olimex but I always get an answer … and they provide quite nice boards so that …

Anyway, I suggested them to provide a board selector in their web to make a quick view of the differences between all the boards … example : size of flash, of ram, ethernet, …

Looks like this board may be ready for sale now. There is no " BOARD WILL BE AVAILABLE FOR SALE " notice on its page anymore.

Sparkfun, is this true and are you going to get them ?