Olimex LPC2148 and IAR Uart example not working

Hi, Has anyone gotten the Olimex LPC2148 development board and IAR Uart example working for the LPC214X? I can see something with hyperterminal, however it is just junk characters. I have tried all available baud rates. Is this code possibly for a specific dev board? This is an initial test to get running, what I really need to do is get FAT16 talking to an sd/MMC card. Is there anything on that while I’m here?

Thanks alot.

are lpc2148 protoboards from olimex already available?

yes, here’s a link.

http://microcontrollershop.com/product_ … ts_id=1183

The uart appears to be working at 28800, hyperterminal didn’t have that baud available.

Steve

Yes, there is a FAT16 implementation that already has support for SD/MMC cards using SPI. Martin Thomas has ported it to LPC and added a little example program. I got his code working relatively easy on my embedded artists development kit.

The efsl project is at http://sf.net/projects/efsl

Check out the “stable” branch, version 0.2.5