olimex SAM9L9260 Restoring linux

I tried to erase and restore my linux from my board but i had some problens

1st - my CD that came with board have NANDFLASH.tcl missing and this

file is required to follow the procedure

2nd - When i follow the procedure defined by olimex i recieve the log file as

follows

-I- Waiting ...
connection : \usb\ARM0
board : AT91SAM9260-EK
target(handle) : 15826304
read chip ID : 0x00000010 at addr: 0xFFFFEE40
read chip ID : 0x019803A1 at addr: 0xFFFFF240
-I- Found processor : AT91SAM9260 (0x019803A0)
-I- Loading applet isp-extram-at91sam9260.bin at address 0x200000
-I- Memory Size : 0x4000000 bytes
-I- Buffer address : 0x2007C4
-I- Buffer size: 0x0 bytes
-I- Applet initialization done
-I- External RAM initialized
script file : at91sam9260_demo_linux_dataflash.tcl
-I- === Initialize the DataFlash access ===
-I- DATAFLASH::Init 1 (trace level : 3)
-I- Loading applet isp-dataflash-at91sam9260.bin at address 0x20000000
-E- Script File at91sam9260_demo_linux_dataflash.tcl returned error : Error Initializing DataFlash Applet (Can't detect known device) - Error Initializing DataFlash Applet (Can't detect known device)
    while executing
"error "Error Initializing DataFlash Applet ($dummy_err)""
    (procedure "DATAFLASH::Init" line 13)
    invoked from within
"DATAFLASH::Init 1 "
    ("AT91C_SPI0_CS1" arm line 1)
    invoked from within
"switch $Dataflash_CS {
            "AT91C_SPI0_CS0"   { DATAFLASH::Init 0 }
            "AT91C_SPI0_CS1"   { DATAFLASH::Init 1 }
            default  ..."
    (procedure "DATAFLASH::SelectDataflash" line 3)
    invoked from within
"DATAFLASH::SelectDataflash AT91C_SPI0_CS1"
    (file "at91sam9260_demo_linux_dataflash.tcl" line 86)
    invoked from within
"source $scriptFile"

So guys I’m here to ask for HELP and if someone have the NANDFLASH.tcl file please send m by e-mail or something

thx i wait response :shock: