Hello,
Please forgive me…
still having problems!
My problem is in reference to a solution provided by a very helpful gentleman known as “Mee_n_Mac”.
Mee_n_Mac, if you are there, I got to say that I need your help! I am sure you remember the previous few post where we discussed about op amp ramps and that you have gracefully provided your help along with other fellows. Well, okay, I now changed the values to actually do the circuit I need for a project, and I don’t get why it doesn’t seem to work. I have followed your instructions of calculating the vo/vin gain, followed by plugging that gain in as K1 (In this case) in the following formula:
Vout=K2V2-K1V1
And then solving for K2… and then the rest to solve for the resistors. I am really upset at myself… I tried several attempts and when I check the values they never work out for both Vouts. :x :x :x
The circuit is an inverting op amp with 2.5 to 2.0 volts ramp at V1 and a steady 5Vdc at V2. Vout should be 0.531Vdc to 1.45Vdc. Therefore, when V1 is 2.5Vdc, the output should be 0.531Vdc. And when V1 goes to 2.0Vdc, the output should be 1.45Vdc.
Please view attachment!
I try and I try and I try just to never be able to prove my findings … very frustrated… Your help is very appreciated!
Thank you!