OpenLog Artemis Crystal Accuracy/Model Number

Hi,

I’m wondering if there is any information on the timing accuracy (say in ppm) or model number of the 32.768 kHz crystal used in the OpenLog Artemis board?

I note from the datasheet, the Apollo MCU can calibrate the XTAL input to +/-1ppm but imagine that the actual accuracy of the crystals are poorer than this.

Thanks in advance,

Jonathan

In the forum post : viewtopic.php?f=169&t=58135 I have attached a document which includes the crystal specification for the Apollo2. I expect it is not different for the Apollo3.

Thanks Paul, it looks like all of those for the Apollo2 have a timing accuracy of +/-20ppm so I’ll run with that.