Hi all.
I have an Openlog Qwiic connected to an Adafruit BNO055 sensor and an Adafruit QT PY (a basic SAMD21 chip).
I can log data but I get random characters missing when I look at the log file.
By my own admission … I’m the worst coder and relatively new at this so any help / guidance much appreciated.
The attached code has been adapted from others sketches.
#include <Wire.h>
#include <Adafruit_Sensor.h>
#include <Adafruit_BNO055.h>
#include <utility/imumaths.h>
#include "SparkFun_Qwiic_OpenLog_Arduino_Library.h"
OpenLog myLog; //Create instance
int ledPin = LED_BUILTIN; //Status LED connected to digital pin 13
  
Adafruit_BNO055 bno = Adafruit_BNO055(55);
void setup(void) 
{
  pinMode(ledPin, OUTPUT);
  Wire.begin(); //Initialize I2C
  myLog.begin(); //Open connection to OpenLog (no pun intended)
  
  Serial.begin(9600);
  Serial.println("Orientation Sensor Test"); Serial.println("");
  
  /* Initialise the sensor */
  if(!bno.begin())
  {
    /* There was a problem detecting the BNO055 ... check your connections */
    Serial.print("Ooops, no BNO055 detected ... Check your wiring or I2C ADDR!");
    while(1);
  }
  
  delay(1000);
    
  bno.setExtCrystalUse(true);
}
void loop(void) 
{
  /* Get a new sensor event */ 
  sensors_event_t event; 
  bno.getEvent(&event);
  
  /* Display the floating point data */
  Serial.print("X: ");
  Serial.print(event.orientation.x, 4);
  Serial.print("\tY: ");
  Serial.print(event.orientation.y, 4);
  Serial.print("\tZ: ");
  Serial.print(event.orientation.z, 4);
  Serial.println("");
  /* Log the floating point data */
  myLog.print("X: ");
  myLog.print(event.orientation.x, 4);
  myLog.print("\tY: ");
  myLog.print(event.orientation.y, 4);
  myLog.print("\tZ: ");
  myLog.print(event.orientation.z, 4);
  myLog.println("");
  
  myLog.syncFile();
  
  delay(100);
}