OpenOCD 0.4.0 cofiguration for OLIMEX ARM-USB-TINY-H

ernestw:
I really need to see the file “at91sam7sx.cfg”

Thank you for your quick reply. I will do what you’re telling me to. :slight_smile:

(I use Mac OS X, which is much closer to Linux than it is to Windows)

-Meanwhile here’s my at91sam7sx.cfg file (I didn’t modify this file at all):

#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config srst_only srst_pulls_trst

if { [info exists CHIPNAME] } {
   set  _CHIPNAME $CHIPNAME
} else {
   set  _CHIPNAME sam7x256
}

if { [info exists ENDIAN] } {
   set  _ENDIAN $ENDIAN
} else {
   set  _ENDIAN little
}

if { [info exists CPUTAPID ] } {
   set _CPUTAPID $CPUTAPID
} else {
   set _CPUTAPID 0x3f0f0f0f
}

jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID

set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME arm7tdmi -endian $_ENDIAN -chain-position $_TARGETNAME -variant arm7tdmi

$_TARGETNAME configure -event reset-init {
	# disable watchdog
	mww 0xfffffd44 0x00008000
	# enable user reset
	mww 0xfffffd08 0xa5000001
	# CKGR_MOR : enable the main oscillator
	mww 0xfffffc20 0x00000601
	sleep 10
	# CKGR_PLLR: 96.1097 MHz
	mww 0xfffffc2c 0x00481c0e
	sleep 10
	# PMC_MCKR : MCK = PLL / 2 ~= 48 MHz
	mww 0xfffffc30 0x00000007
	sleep 10
	# MC_FMR: flash mode (FWS=1,FMCN=60)
	mww 0xffffff60 0x003c0100
	sleep 100
}

$_TARGETNAME configure -work-area-phys 0x00200000 -work-area-size 0x4000 -work-area-backup 0

#flash bank <driver> <base_addr> <size> <chip_width> <bus_width> <target_number> [<target_name> <banks> <sectors_per_bank> <pages_per_sector> <page_size> <num_nvmbits> <ext_freq_khz>]
set _FLASHNAME $_CHIPNAME.flash
flash bank $_FLASHNAME at91sam7 0 0 0 0 $_TARGETNAME 0 0 0 0 0 0 0 18432

# For more information about the configuration files, take a look at:
# openocd.texi

The flash line differs quite a lot from what it should be then.

I believe this message…

flash write_bank 0 Example.bin 0x0: command requires more arguments

…most likely comes from one of the environment variables not being defined. I’ll try and find out which one.