I have an issue when i start up openocd .
i get:
root@kali:/opt/openocd-code# openocd
Open On-Chip Debugger 0.10.0-dev-00022-g2dcf7bf-dirty (2015-08-15-20:27)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
embedded:startup.tcl:60: Error: Can’t find openocd.cfg
in procedure ‘script’
at file “embedded:startup.tcl”, line 60
Error: Debug Adapter has to be specified, see “interface” command
embedded:startup.tcl:60: Error:
in procedure ‘script’
at file “embedded:startup.tcl”, line 60
and my usb jtag is :
Bus 001 Device 003: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
How should i configure openocd.cfg file and where did i put it ?
My target is a broadcom 63281
Note : It looks that openocd is unable to open the jtag programmer , anyway , i have made a pastebin file with all log since the installation until this error appear , just in case any of you could give a look and figure out what is going on here :
URJtag detects the usb jtag programmer but is unable to get a connection with the broadcom processor .
the pastebin is here from URjtag http://pastebin.com/yXm9tqwC