Hi Guys,
I’m trying to use openOCD to debug a custom board(NavStik, see http://navstik.org/home/), implementing:
FTDI FT4232H
STM32F407
I’ve built the newest libusb (with --enable-ftdi) and run ubuntu 14.04(64 bits).
This is the command I give:
sudo openocd -f ~/Downloads/openocd.8.0/tcl/interface/ftdi/openocd-usb-hs.cfg
-f ~/Downloads/openocd-0.8.0/tcl/target/stm32f4x.cfg
I have modified openocd-usb-hs.cfg as follows:
gdb_port 3333
#tcl_port 6666
telnet_port 4444
interface ftdi
#ftdi_device_desc “Dual RS232-HS”
ftdi_vid_pid 0x0403 0x6011
debug_level 2
And this is the response:
debug_level: 2
adapter speed: 3000 kHz
adapter_nsrst_delay: 200
jtag_ntrst_delay: 200
Warn : target name is deprecated use: ‘cortex_m’
Info : clock speed 3000 kHz
Error: JTAG scan chain interrogation failed: all ones
Error: Check JTAG interface, timings, target power, etc.
Error: Trying to use configured scan chain anyway…
Error: stm32f4xxx.cpu: IR capture error; saw 0x0f not 0x01
Warn : Bypassing JTAG setup events due to errors
Warn : Invalid ACK 0x7 in JTAG-DP transaction
When increasing the debug level to 3, I get (prior to the first error):
Debug: 177 410 command.c:145 script_debug(): command - ocd_jtag ocd_jtag arp_init
Debug: 178 410 core.c:1417 jtag_init_inner(): Init JTAG chain
Debug: 179 410 core.c:323 jtag_call_event_callbacks(): jtag event: TAP reset
Debug: 180 410 core.c:1048 jtag_examine_chain(): DR scan interrogation for IDCODE/BYPASS
Debug: 181 410 core.c:323 jtag_call_event_callbacks(): jtag event: TAP reset
Error: 182 411 core.c:941 jtag_examine_chain_check(): JTAG scan chain interrogation failed: all ones
I’ve tried the following:
-
using openOCD-0.7.0, which gives me the same, only it keeps trying to poll the CPU.
-
adapter speeds 3000KHz and 2000KHz and jtag and adapter delays of 100.
-
do a reset in the configure script but to no avail.
(Is there anything else you recommend trying?)
When searching ‘the internet’, this error seems to indicate a physical problem.
(I’m not sure how much it matters, but is the fact that this chip has 4 COM-ports any complication in this?)
I’ve already contacted the manufacturer, but before giving up on this board I would like to ask you guys:
Does there happen to be a (known)bug or something in the configuration, openOCD, or should I just assume my hardware is broken(I have no way to really test it here…)?
I’m hoping to hear from you, thanks in advance.
153rd