I am trying to test source level debugging with a OLimex ARM-USB-OCD-H jtag adapter and my Intel Galileo Gen 2 board but when i try to start openocd I get
openocd -f /usr/share/openocd/scripts/interface/ftdi/olimex_arm_usb_ocd_h.cfg -f /usr/share/openocd/scripts/board/quark_x10xx,board.cfg
Open On_Chip Debugger 0.8.0 (2017-06-26-22:51)
Licensed under GNU GPL v2
Info: only one transport option: autoselect ‘jtag’
adapter speed: 4000 kHz
trst_only separate trst_push_pull
Info: clock speed 4000 kHz
Info: JTAG tap;quark_x10xx.cltap tap/device found 0x0e681013 (mfg:0x009,port:0xe681, ver: 0x0)
Error: quark_x10xx.cltap: IR capture error: saw 0xff not0x1
Warn: Bypassing JATG setup events due to error
Pls can you help me to solve the problem?
Best regards and thanks in advance