Openocd STR912 JTAG key

Hello,

I currently try to set up a system consisting out of Eclipse (YAGARTO) STR12 and the JTAG key of amontec. when I run the Config file I receive the Error messeag:

Info: openocd.c:93 main(): Open On-Chip Debugger (2007-12-30 17:00 CET) svn: 247

Info: openocd.c:94 main(): $URL: http://svn.berlios.de/svnroot/repos/ope … /openocd.c $

Info: jtag.c:1291 jtag_examine_chain(): JTAG device found: 0x04570041 (Manufacturer: 0x020, Part: 0x4570, Version: 0x0)

Info: jtag.c:1291 jtag_examine_chain(): JTAG device found: 0x25966041 (Manufacturer: 0x020, Part: 0x5966, Version: 0x2)

Info: jtag.c:1291 jtag_examine_chain(): JTAG device found: 0x2457f041 (Manufacturer: 0x020, Part: 0x457f, Version: 0x2)

Warning: arm7_9_common.c:682 arm7_9_poll(): DBGACK set while target was in unknown state. Reset or initialize target before resuming

Warning: arm7_9_common.c:941 arm7_9_halt(): target was already halted

my config file looks like this

#daemon configuration

telnet_port 4444

gdb_port 3333

#interface

interface ft2232

ft2232_device_desc “Amontec JTAGkey A”

ft2232_layout jtagkey

jtag_speed 1000

#jtag_nsrst_delay 200

#jtag_ntrst_delay 200

#use combined on interfaces or targets that can’t set TRST/SRST separately

reset_config trst_and_srst

#jtag scan chain

#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)

jtag_device 8 0x1 0x1 0xfe

jtag_device 4 0x1 0xf 0xe

jtag_device 5 0x1 0x1 0x1e

#target configuration

daemon_startup reset

#target

#target arm966e

target arm966e little reset_halt 1 arm966e

run_and_halt_time 0 30

#working_area 0 0x50000000 16384 nobackup

#flash bank <chip_width> <bus_width>

#flash bank str9x 0x00000000 0x00080000 0 0 0

#Script used for FLASH erasing

#target_script 0 reset C:\OpenOCD_Skript\str91x_flasherase.ocd

can anyone provid me with help?