OpenOCD XSVF: cmd over several lines.

Hi at all,

I’m new at OOCD and a try to load a Spartan 3A with the XSVF-Player. It seems all good until the parser get a cmd, which is over several lines.

for example of the svf-file:

SDR 8197344 TDI (0004000400040004000400040004000400040004000400040004000400040004b000850cd968b800400c8100830c8100870ca000850c0004000400040004c000850c5000850cb749d400400c000000000000000000000000000000000000000000000000000000000000000000000000000000

000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000…

…ffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff) ;

(the file was transfer from svf to xsvf by xilinx’s svf2xsvf)

can oocd only work with cmd’s which contains max 256 char (a line in a svf-file has max. 256 char or several lines are a pair of the cmd)

thanks for answer