Original redboard gets port unavailable message

Hello!

I own one of the original Redboards as sold via MicroCenter for Sparkfun. On this laptop who runs Windows 11 I am now getting output which looks like this:



FQBN: SparkFun:avr:RedBoard
Using board ‘uno’ from platform in folder: C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6
Using core ‘arduino’ from platform in folder: C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6
Detecting libraries used…
C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-g++ -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10607 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR -IC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6\cores\arduino -IC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6\variants\standard C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8\sketch\Blink.ino.cpp -o nul
Generating function prototypes…
C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-g++ -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10607 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR -IC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6\cores\arduino -IC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6\variants\standard C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8\sketch\Blink.ino.cpp -o C:\Users\hanso\AppData\Local\Temp\3100735918\sketch_merged.cpp
C:\Users\hanso\AppData\Local\Arduino15\packages\builtin\tools\ctags\5.8-arduino11/ctags -u --language-force=c++ -f - --c+±kinds=svpf --fields=KSTtzns --line-directives C:\Users\hanso\AppData\Local\Temp\3100735918\sketch_merged.cpp
Compiling sketch…
“C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -MMD -flto -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10607 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6\cores\arduino” “-IC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.8.6\variants\standard” “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8\sketch\Blink.ino.cpp” -o “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8\sketch\Blink.ino.cpp.o”
Compiling libraries…
Compiling core…
Using precompiled core: C:\Users\hanso\AppData\Local\arduino\cores\arduino_avr_uno_575a166275f464c037e04c27f2d5372d\core.a
Linking everything together…
“C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-gcc” -w -Os -g -flto -fuse-linker-plugin -Wl,–gc-sections -mmcu=atmega328p -o “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.elf” “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8\sketch\Blink.ino.cpp.o” “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/..\..\cores\arduino_avr_uno_575a166275f464c037e04c27f2d5372d\core.a” “-LC:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8” -lm
“C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-objcopy” -O ihex -j .eeprom --set-section-flags=.eeprom=alloc,load --no-change-warnings --change-section-lma .eeprom=0 “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.elf” “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.eep”
“C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-objcopy” -O ihex -R .eeprom “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.elf” “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.hex”
“C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7/bin/avr-size” -A “C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.elf”
Sketch uses 924 bytes (2%) of program storage space. Maximum is 32256 bytes.
Global variables use 9 bytes (0%) of dynamic memory, leaving 2039 bytes for local variables. Maximum is 2048 bytes.
“C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino17/bin/avrdude” “-CC:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino17/etc/avrdude.conf” -v -V -patmega328p -carduino “-PCOM4” -b115200 -D “-Uflash:w:C:\Users\hanso\AppData\Local\arduino\sketches\EF8C8743265BF0EFC51680A7C41DAFF8/Blink.ino.hex:i”

`avrdude: Version 6.3-20190619

``Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/

Copyright (c) 2007-2014 Joerg Wunsch

     System wide configuration file is "C:\Users\hanso\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino17/etc/avrdude.conf"

     Using Port                    : COM4
     Using Programmer              : arduino
     Overriding Baud Rate          : 115200

avrdude: ser_open(): can’t open device “\.\COM4”: Access is denied.

avrdude done. Thank you.

Failed uploading: uploading error: exit status 1

Anyway that happens on both 2.3.6 and 2.3.7.



1- Are you sure the board is actually on com4?
2- Does it work on another computer?

It is indeed on COM4. However I’m away at the moment, and do not have another one to try it out on. However the code that I was trying to make work, did work on an older version.

Did you get this goin’?

Hello!

Oh yes. The solution was indeed to make use of an older release. The last of the 1.8 releases before moving to this series was the ticket.