Package Tracking and LPC2148

Hi,

The Package Tracking module comes with a LPC2184. When I do a search on SparkFun I get the following chip: ALFATxp LPC2148 FAT IC. Is this the same chip?

When it is, is it true that the product is discontinued? If so, which chip will come in place?

If not wich chip would it be in that case?

Thanks!

Roel Alblas

That sparkfun product is a pre-programmed LPC2148.

The LPC2148 is made by NXP (formerly Phillips)

Copy this whole line into your browser:

http://www.nxp.com/#/pip/pip=[pip=LPC2141_42_44_46_48_4]|pp=[t=pip,i=LPC2141_42_44_46_48_4]

Thanks for your quick reply! I know where to look now.

Could I replace it with the one I showed?

Roel

Its the same part…

The package tracker firmware files (available as open source) already contain a FAT16 and SD card driver…