Hello,
I’m getting ready to send a first order: a simple 2-layer, 1.0 X 1.0 inch board. Since I had some place left in my original layout, I decided to place a SSOP8 footprint in the empty corner, wired to pin headers. This SSOP8-to-DIP converter is for another project, so I want it cut off from the main board.
To do this, 2 things aren’t clear to me, even after reading the FAQ, the Eagle tutorial, and a number of threads on this forum:
1-
Where and how do I specify the external border for the whole circuit? In my case, this is the 1 X 1 inch square that I’ll be charged for (hopefully!)
I know I put a rectangle in the 20-Dimension layer (I’m using eagle-4.13), but it doesn’t show up when I import my gerbers in Viewmate.
2-
As for that piggyback footprint, can SFE do what I want? If so, how do I specify it in the required gerbers? I thought I could put lines in the Milling layer, but it didn’t look too kosher… I have no idea if sparkfun’s CAM file takes care of routing and milling guides.
I was going to attach a gif of what I want to do, but I didn’t find out how… here’s a link instead:
http://rsc-mirror3.netfirms.com/2/sq.htm
I hope it’s clear enough! if not, I can upload my gerbers, or a screenshot of my layout, or whatever…
As I said I read the FAQ, the Eagle tutorial and quite a few threads on this forum, but I didn’t find any satisfying answer…
Maybe I should email my .brd file to spark@sparfun and say “I need 21 copies of this 3-layer board by monday, with 45° stripes of blue and red soldermask on every alternating odd-numbered copy… BTW, what is a Gerber???”
![]()
thanks for any info,
Christian