Hello All,
I’m trying to use a PCF8575C port expander to drive 16 LED’s. I found this demo (which uses PCF8575) http://www.youtube.com/watch?v=UXPuzbEV … ture=email that turns on each LED in series, but I’m unable to get it to work. This what I have at present
http://www.lucadentella.it/blog/wp-cont … 00x228.jpg : (Arduino) PIN A4 → (PCF8575) PIN SDA
(Arduino) PIN A5 → (PCF8575) PIN SCL
(Arduino) PIN 5V → (PCF8575) PIN VCC
(Arduino) PIN GND → (PCF8575) PIN GND
(Arduino) PIN GND → (PCF8575) PIN A0, A1, A2
That’s the way it’s setup in the demo and in the makers blog http://www.lucadentella.it/2012/03/16/o … xpander/3/, yet I don’t get any response from the LED’s.
Here’s the code:
First off I was unable to get it to compile, after look at afew other code snippets I changed
to
and was able to get it to compile, but still not a blink from an LED.
The breakout board’s datasheet says Pin connections:
SDA to pin 4 on the analog header
SCL to pin 5 on the analog header
VCC to 5v
GND to GND
I/O pins need pull up resistors to VCC.
I didn’t use any resistors because the demo didn’t include them. What am I doing?
so far this is whats I’ve found:
• Difference between PCF8575 and PCF8575C are:
– No internal I/O current source (open-drain)
– TTL input levels
http://ics.nxp.com/support/documents/in … /an469.pdf
- Question: In the data sheet of PCF8575 it is mentioned that the Port output is HIGH
after power-on. In the data sheet of PCF8575C it is mentioned that the Port output will
be in 3-state condition after power-on. We found that there is no difference in the block
diagram and the simplified schematic diagram of each I/O. What is the condition of the
outputs after power-on?
Answer: There is in fact a small difference in the schematic diagrams for PCF8575
and PCF8575C. The PCF8575C lacks the weak pull-up in the form of the 100 μA
current source in the output I/Os. This is the reason that PCF8575’s I/Os remain HIGH
after power-on and after being written HIGH. Without this current source, PCF8575C’s
I/Os will be in high-impedance state after the initial strong pull-up transistor is OFF (it
is ON during the acknowledge phase)
http://www.electro-tech-online.com/gene … -high.html
I’m not exactly sure hot to compensate for this difference.
If anyone can help it will be greatly appreciated.
Thank you in advance