Permanent Change to Airspeed on LoRaSerial

I am trying to use the LoRa Serial kit to transmit base corrections between two RTK Postcards. I am struggling to get consistent communication.

I am running V2.3 RTK Everywhere on the postcards and V6 on the LG290P. The LoRa are connected directly through the UART3 on the Postcard.

The LG290P does not support 57600 bps on the UART3 so I have changed the Postcard to use 115200 bps on the UART3.

Given that the default for the LoRa is 57600, I need to permanently change this on the LoRa.

As well, doing the calc, it seems as though the default air speed baud rate of the LoRa is not fast enough (4800). I’d like to set it to its max speed of 19200 as my distance is less than 1km with good LoS between the base and the rover.

I have been able to permanently set the serial speed to 115200 bps in part by following this thread.

However, using the same AT commands, I can’t permanently set the airspeed to 19200. Sometimes it takes me 1 or 2 tries before it will show me that its set to 19200. However when I power cycle it always resets to 0 which I assume is default - 4800. I am using the following AT commands:

+++

AT-AirSpeed=19200

(it will give me a warning about changing 5 parameters)

ATW

ATI0 (to check - typically it shows 19200 at this point)

ATO

power cycle

+++

ATI0 (to check - it always shows 0 after the power cycle)

Can someone provide assistance on how to make this change permanent?

Thanks,

Paul

undocumented but reliable...

$PQTMCFGUART,W,3,57600*34

TCIII did it & solved.

Thanks @bamarcant but I don’t have an issue (I don’t think) with using 115200 for my UART3. Just with permanently upping my airspeed on my LoRa.

I’m a rookie at this stuff so happy to be corrected.

Ryan (@AORPLS ) can give you clarifications on the matter…
Regards

If I recall and it’s been a while there was something to do with forcing it to write the config multiple times for airspeed to stick.

@bamarcant

That is correct. I have two LG290P Rovers set to 57600 baud on UART3 for receiving incoming RTCM3 messages from my Postcard Base Station that is transmitting on UART3 at 57600 baud.

TCIII

I know there has been debate on whether the LG290P Quectel’s are compatible with 57600 baud but now the RTK Everywhere v2.3 says that 57600 is out of range. You can only have 9600 or 115200 (or higher).

The only thing I have found for the airspeed to stick is to change the underlying parameters - bandwidth, coding rate, spreadfactor, RxToTxUsec, Heartbeattimeout. When these are changed (and you enter the commands ATW, ATO), it will change them permanently even after a power cycle.

Unfortunately these changes, plus others like turning of encryption, turning off frequency hops to try and make the comms as fast and as robust as possible has not helped. I still can’t good enough communication between my Base and Rover to get RTK-Fix.

For anyone who has, I’d love to see what you have your settings as I’ve tried everything I’m aware of (detailed in this thread)

just a follow up that I finally got these to work as detailed in this thread