I’m looking for a miniature RGB camera module similar to those used in the PiCam V2 (Sony IMX219) or the Coral Camera (Omnivision OV5645), for a machine vision application. For ergonomic reasons, I need to use an IR illuminator instead of a visible-light LED strobe.
Do either of these camera modules have IR sensitivity, and if not, are any RGB camera modules of similar type available that can also see in the IR? (NOTE: Thermal imaging cameras aren’t useful here, as I need visible-light imaging as well as IR.) Some cell phone cameras provide an IR mode, so this should be possible…