Hi,
I am wondering wether I can use the 5V output on the MicroView to power the Qwiic Scale - NAU7802?
I realise the NAU7802 is supposed to be used with 3.3V but in the Datasheet it is mentioned that an Inputvoltage of 2.7V~5.5V can be used. I have tested it and the LED lights up but I can’t communicate with it. The board isn’t fried as it still works perfectly when I connect it to a 3.3V power supply.
Is there anything specific I have to do (i.e. clip a jumper) to make it work with a 5V Input or do I have to use a level shifter?