problem arduino 22

i an trying to code for micro sd on arduino nanO 328 by arduino 22

and when a resolve many many many ( 200 errors very code it’s just adaptation code)

at the then i just have an error very horrible i let you see:

In file included from ProjetCanSat2011.cpp:12:c:/program files (x86)/arduino-0022/hardware/tools/avr/lib/gcc/…/…/avr/include/SDCard/FAT32.h:

In function ‘void displayMemory(unsigned char, long unsigned int)’:c:/program files (x86)/arduino-0022/hardware/tools/avr/lib/gcc/…/…/avr/include/SDCard/FAT32.h:343: error: call of overloaded ‘print(unsigned char [20])’ is ambiguous

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:44: note: candidates are: void Print::print(const String&)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:45: note: void Print::print(const char*)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:46: note: void Print::print(char, int)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:47: note: void Print::print(unsigned char, int)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:48: note: void Print::print(int, int)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:49: note: void Print::print(unsigned int, int)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:50: note: void Print::print(long int, int)

C:\Program Files (x86)\arduino-0022\hardware\arduino\cores\arduino/Print.h:51: note: void Print::print(long unsigned int, int)

you can see the difference enter C:/ and C:\ i don’t find the FAT32 what is here c:/program files (x86)/arduino-0022/hardware/tools/avr/lib/gcc/…/…/avr/include/SDCard/FAT32.h

So how i do to resolve my problem?? think very much for the person who find solution.