Problem getting blink_1MHz and @mega328

First off, here is my environment:

Gentoo Linux (kernel 2.6.36-gentoo-r5)

avr-gcc 4.5.2

avrdude 5.5

Updated avrdude.conf for atmega328p

Atmega328p microcontroller

So I went through the sparkfun tutorial, connected everything.

I then went and compiled blink_1MHz.c (successfully).

Then I ran avrdude (after configuration) using

make program

and it looks like avrdude completes successfully

avrdude -p atmega328p -P /dev/parport0 -c stk200 -v -v -U flash:w:blink_1MHz.hex

avrdude: Version 5.5, compiled on Mar 5 2011 at 19:58:36

Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/

System wide configuration file is “/etc/avrdude.conf”

User configuration file is “/home/cwinters/.avrduderc”

User configuration file does not exist or is not a regular file, skipping

Using Port : /dev/parport0

Using Programmer : stk200

AVR Part : ATMEGA328P

Chip Erase delay : 9000 us

PAGEL : PD7

BS2 : PC2

RESET disposition : dedicated

RETRY pulse : SCK

serial program mode : yes

parallel program mode : yes

Timeout : 200

StabDelay : 100

CmdexeDelay : 25

SyncLoops : 32

ByteDelay : 0

PollIndex : 3

PollValue : 0x53

Memory Detail :

Block Poll Page Polled

Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack


eeprom 65 5 4 0 no 1024 4 0 3600 3600 0xff 0xff

flash 65 6 128 0 yes 32768 128 256 4500 4500 0xff 0xff

lfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00

hfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00

efuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00

lock 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00

calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00

signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00

Programmer Type : PPI

Description : STK200

VCC = (not used)

BUFF = 4,5

RESET = 9

SCK = 6

MOSI = 7

MISO = 10

ERR LED = 0

RDY LED = 0

PGM LED = 0

VFY LED = 0

avrdude: Calibrating delay loop… calibrated to 499 cycles per us

bitbang_cmd(): [ AC 53 00 00 ] [ FF FF 53 00 ]

avrdude: AVR device initialized and ready to accept instructions

Reading | bitbang_cmd(): [ 30 00 00 00 ] [ 00 30 00 1E ]

bitbang_cmd(): [ 30 00 01 00 ] [ 00 30 00 95 ]

################bitbang_cmd(): [ 30 00 02 00 ] [ 00 30 00 0F ]

################################## | 100% 0.00s

avrdude: Device signature = 0x1e950f

bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]

bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]

bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]

avrdude: safemode: lfuse reads as 62

bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]

bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]

bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]

avrdude: safemode: hfuse reads as D9

bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]

bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]

bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]

avrdude: safemode: efuse reads as 7

avrdude: NOTE: FLASH memory has been specified, an erase cycle will be performed

To disable this feature, specify the -D option.

bitbang_cmd(): [ A0 03 FC 00 ] [ 00 A0 03 FF ]

bitbang_cmd(): [ A0 03 FD 00 ] [ 00 A0 03 FF ]

bitbang_cmd(): [ A0 03 FE 00 ] [ 00 A0 03 FF ]

bitbang_cmd(): [ A0 03 FF 00 ] [ 00 A0 03 FF ]

avrdude: erasing chip

bitbang_cmd(): [ AC 80 00 00 ] [ 00 AC 80 00 ]

avrdude: Calibrating delay loop… calibrated to 497 cycles per us

bitbang_cmd(): [ AC 53 00 00 ] [ FF FF 53 00 ]

avrdude: reading input file “blink_1MHz.hex”

avrdude: input file blink_1MHz.hex auto detected as Intel Hex

avrdude: writing flash (248 bytes):

Writing | bitbang_cmd(): [ 40 00 00 0C ] [ 00 40 00 00 ]

bitbang_cmd(): [ 48 00 00 94 ] [ 0C 48 00 00 ]

bitbang_cmd(): [ 40 00 01 34 ] [ 94 40 00 01 ]

bitbang_cmd(): [ 48 00 01 00 ] [ 34 48 00 01 ]

bitbang_cmd(): [ 40 00 02 0C ] [ 00 40 00 02 ]

#bitbang_cmd(): [ 48 00 02 94 ] [ 0C 48 00 02 ]

bitbang_cmd(): [ 40 00 03 51 ] [ 94 40 00 03 ]

bitbang_cmd(): [ 48 00 03 00 ] [ 51 48 00 03 ]

bitbang_cmd(): [ 40 00 04 0C ] [ 00 40 00 04 ]

bitbang_cmd(): [ 48 00 04 94 ] [ 0C 48 00 04 ]

#bitbang_cmd(): [ 40 00 05 51 ] [ 94 40 00 05 ]

bitbang_cmd(): [ 48 00 05 00 ] [ 51 48 00 05 ]

bitbang_cmd(): [ 40 00 06 0C ] [ 00 40 00 06 ]

bitbang_cmd(): [ 48 00 06 94 ] [ 0C 48 00 06 ]

bitbang_cmd(): [ 40 00 07 51 ] [ 94 40 00 07 ]

#bitbang_cmd(): [ 48 00 07 00 ] [ 51 48 00 07 ]

bitbang_cmd(): [ 40 00 08 0C ] [ 00 40 00 08 ]

bitbang_cmd(): [ 48 00 08 94 ] [ 0C 48 00 08 ]

bitbang_cmd(): [ 40 00 09 51 ] [ 94 40 00 09 ]

bitbang_cmd(): [ 48 00 09 00 ] [ 51 48 00 09 ]

#bitbang_cmd(): [ 40 00 0A 0C ] [ 00 40 00 0A ]

bitbang_cmd(): [ 48 00 0A 94 ] [ 0C 48 00 0A ]

bitbang_cmd(): [ 40 00 0B 51 ] [ 94 40 00 0B ]

bitbang_cmd(): [ 48 00 0B 00 ] [ 51 48 00 0B ]

bitbang_cmd(): [ 40 00 0C 0C ] [ 00 40 00 0C ]

#bitbang_cmd(): [ 48 00 0C 94 ] [ 0C 48 00 0C ]

bitbang_cmd(): [ 40 00 0D 51 ] [ 94 40 00 0D ]

bitbang_cmd(): [ 48 00 0D 00 ] [ 51 48 00 0D ]

bitbang_cmd(): [ 40 00 0E 0C ] [ 00 40 00 0E ]

bitbang_cmd(): [ 48 00 0E 94 ] [ 0C 48 00 0E ]

#bitbang_cmd(): [ 40 00 0F 51 ] [ 94 40 00 0F ]

bitbang_cmd(): [ 48 00 0F 00 ] [ 51 48 00 0F ]

bitbang_cmd(): [ 40 00 10 0C ] [ 00 40 00 10 ]

bitbang_cmd(): [ 48 00 10 94 ] [ 0C 48 00 10 ]

bitbang_cmd(): [ 40 00 11 51 ] [ 94 40 00 11 ]

#bitbang_cmd(): [ 48 00 11 00 ] [ 51 48 00 11 ]

bitbang_cmd(): [ 40 00 12 0C ] [ 00 40 00 12 ]

bitbang_cmd(): [ 48 00 12 94 ] [ 0C 48 00 12 ]

bitbang_cmd(): [ 40 00 13 51 ] [ 94 40 00 13 ]

bitbang_cmd(): [ 48 00 13 00 ] [ 51 48 00 13 ]

#bitbang_cmd(): [ 40 00 14 0C ] [ 00 40 00 14 ]

bitbang_cmd(): [ 48 00 14 94 ] [ 0C 48 00 14 ]

bitbang_cmd(): [ 40 00 15 51 ] [ 94 40 00 15 ]

bitbang_cmd(): [ 48 00 15 00 ] [ 51 48 00 15 ]

bitbang_cmd(): [ 40 00 16 0C ] [ 00 40 00 16 ]

#bitbang_cmd(): [ 48 00 16 94 ] [ 0C 48 00 16 ]

bitbang_cmd(): [ 40 00 17 51 ] [ 94 40 00 17 ]

bitbang_cmd(): [ 48 00 17 00 ] [ 51 48 00 17 ]

bitbang_cmd(): [ 40 00 18 0C ] [ 00 40 00 18 ]

bitbang_cmd(): [ 48 00 18 94 ] [ 0C 48 00 18 ]

#bitbang_cmd(): [ 40 00 19 51 ] [ 94 40 00 19 ]

bitbang_cmd(): [ 48 00 19 00 ] [ 51 48 00 19 ]

bitbang_cmd(): [ 40 00 1A 0C ] [ 00 40 00 1A ]

bitbang_cmd(): [ 48 00 1A 94 ] [ 0C 48 00 1A ]

bitbang_cmd(): [ 40 00 1B 51 ] [ 94 40 00 1B ]

#bitbang_cmd(): [ 48 00 1B 00 ] [ 51 48 00 1B ]

bitbang_cmd(): [ 40 00 1C 0C ] [ 00 40 00 1C ]

bitbang_cmd(): [ 48 00 1C 94 ] [ 0C 48 00 1C ]

bitbang_cmd(): [ 40 00 1D 51 ] [ 94 40 00 1D ]

bitbang_cmd(): [ 48 00 1D 00 ] [ 51 48 00 1D ]

#bitbang_cmd(): [ 40 00 1E 0C ] [ 00 40 00 1E ]

bitbang_cmd(): [ 48 00 1E 94 ] [ 0C 48 00 1E ]

bitbang_cmd(): [ 40 00 1F 51 ] [ 94 40 00 1F ]

bitbang_cmd(): [ 48 00 1F 00 ] [ 51 48 00 1F ]

bitbang_cmd(): [ 40 00 20 0C ] [ 00 40 00 20 ]

#bitbang_cmd(): [ 48 00 20 94 ] [ 0C 48 00 20 ]

bitbang_cmd(): [ 40 00 21 51 ] [ 94 40 00 21 ]

bitbang_cmd(): [ 48 00 21 00 ] [ 51 48 00 21 ]

bitbang_cmd(): [ 40 00 22 0C ] [ 00 40 00 22 ]

bitbang_cmd(): [ 48 00 22 94 ] [ 0C 48 00 22 ]

#bitbang_cmd(): [ 40 00 23 51 ] [ 94 40 00 23 ]

bitbang_cmd(): [ 48 00 23 00 ] [ 51 48 00 23 ]

bitbang_cmd(): [ 40 00 24 0C ] [ 00 40 00 24 ]

bitbang_cmd(): [ 48 00 24 94 ] [ 0C 48 00 24 ]

bitbang_cmd(): [ 40 00 25 51 ] [ 94 40 00 25 ]

#bitbang_cmd(): [ 48 00 25 00 ] [ 51 48 00 25 ]

bitbang_cmd(): [ 40 00 26 0C ] [ 00 40 00 26 ]

bitbang_cmd(): [ 48 00 26 94 ] [ 0C 48 00 26 ]

bitbang_cmd(): [ 40 00 27 51 ] [ 94 40 00 27 ]

bitbang_cmd(): [ 48 00 27 00 ] [ 51 48 00 27 ]

#bitbang_cmd(): [ 40 00 28 0C ] [ 00 40 00 28 ]

bitbang_cmd(): [ 48 00 28 94 ] [ 0C 48 00 28 ]

bitbang_cmd(): [ 40 00 29 51 ] [ 94 40 00 29 ]

bitbang_cmd(): [ 48 00 29 00 ] [ 51 48 00 29 ]

bitbang_cmd(): [ 40 00 2A 0C ] [ 00 40 00 2A ]

#bitbang_cmd(): [ 48 00 2A 94 ] [ 0C 48 00 2A ]

bitbang_cmd(): [ 40 00 2B 51 ] [ 94 40 00 2B ]

bitbang_cmd(): [ 48 00 2B 00 ] [ 51 48 00 2B ]

bitbang_cmd(): [ 40 00 2C 0C ] [ 00 40 00 2C ]

bitbang_cmd(): [ 48 00 2C 94 ] [ 0C 48 00 2C ]

#bitbang_cmd(): [ 40 00 2D 51 ] [ 94 40 00 2D ]

bitbang_cmd(): [ 48 00 2D 00 ] [ 51 48 00 2D ]

bitbang_cmd(): [ 40 00 2E 0C ] [ 00 40 00 2E ]

bitbang_cmd(): [ 48 00 2E 94 ] [ 0C 48 00 2E ]

bitbang_cmd(): [ 40 00 2F 51 ] [ 94 40 00 2F ]

#bitbang_cmd(): [ 48 00 2F 00 ] [ 51 48 00 2F ]

bitbang_cmd(): [ 40 00 30 0C ] [ 00 40 00 30 ]

bitbang_cmd(): [ 48 00 30 94 ] [ 0C 48 00 30 ]

bitbang_cmd(): [ 40 00 31 51 ] [ 94 40 00 31 ]

bitbang_cmd(): [ 48 00 31 00 ] [ 51 48 00 31 ]

#bitbang_cmd(): [ 40 00 32 0C ] [ 00 40 00 32 ]

bitbang_cmd(): [ 48 00 32 94 ] [ 0C 48 00 32 ]

bitbang_cmd(): [ 40 00 33 51 ] [ 94 40 00 33 ]

bitbang_cmd(): [ 48 00 33 00 ] [ 51 48 00 33 ]

bitbang_cmd(): [ 40 00 34 11 ] [ 00 40 00 34 ]

#bitbang_cmd(): [ 48 00 34 24 ] [ 11 48 00 34 ]

bitbang_cmd(): [ 40 00 35 1F ] [ 24 40 00 35 ]

bitbang_cmd(): [ 48 00 35 BE ] [ 1F 48 00 35 ]

bitbang_cmd(): [ 40 00 36 CF ] [ BE 40 00 36 ]

bitbang_cmd(): [ 48 00 36 EF ] [ CF 48 00 36 ]

#bitbang_cmd(): [ 40 00 37 D8 ] [ EF 40 00 37 ]

bitbang_cmd(): [ 48 00 37 E0 ] [ D8 48 00 37 ]

bitbang_cmd(): [ 40 00 38 DE ] [ E0 40 00 38 ]

bitbang_cmd(): [ 48 00 38 BF ] [ DE 48 00 38 ]

bitbang_cmd(): [ 40 00 39 CD ] [ BF 40 00 39 ]

#bitbang_cmd(): [ 48 00 39 BF ] [ CD 48 00 39 ]

bitbang_cmd(): [ 40 00 3A 11 ] [ BF 40 00 3A ]

bitbang_cmd(): [ 48 00 3A E0 ] [ 11 48 00 3A ]

bitbang_cmd(): [ 40 00 3B A0 ] [ E0 40 00 3B ]

bitbang_cmd(): [ 48 00 3B E0 ] [ A0 48 00 3B ]

#bitbang_cmd(): [ 40 00 3C B1 ] [ E0 40 00 3C ]

bitbang_cmd(): [ 48 00 3C E0 ] [ B1 48 00 3C ]

bitbang_cmd(): [ 40 00 3D E8 ] [ E0 40 00 3D ]

bitbang_cmd(): [ 48 00 3D EF ] [ E8 48 00 3D ]

#bitbang_cmd(): [ 40 00 3E F0 ] [ EF 40 00 3E ]

bitbang_cmd(): [ 48 00 3E E0 ] [ F0 48 00 3E ]

bitbang_cmd(): [ 40 00 3F 02 ] [ E0 40 00 3F ]

bitbang_cmd(): [ 48 00 3F C0 ] [ 02 48 00 3F ]

bitbang_cmd(): [ 4C 00 00 00 ] [ C0 4C 00 00 ]

bitbang_cmd(): [ 40 00 00 05 ] [ 00 40 00 00 ]

#bitbang_cmd(): [ 48 00 00 90 ] [ 05 48 00 00 ]

bitbang_cmd(): [ 40 00 01 0D ] [ 90 40 00 01 ]

bitbang_cmd(): [ 48 00 01 92 ] [ 0D 48 00 01 ]

bitbang_cmd(): [ 40 00 02 A0 ] [ 92 40 00 02 ]

bitbang_cmd(): [ 48 00 02 30 ] [ A0 48 00 02 ]

#bitbang_cmd(): [ 40 00 03 B1 ] [ 30 40 00 03 ]

bitbang_cmd(): [ 48 00 03 07 ] [ B1 48 00 03 ]

bitbang_cmd(): [ 40 00 04 D9 ] [ 07 40 00 04 ]

bitbang_cmd(): [ 48 00 04 F7 ] [ D9 48 00 04 ]

bitbang_cmd(): [ 40 00 05 11 ] [ F7 40 00 05 ]

#bitbang_cmd(): [ 48 00 05 E0 ] [ 11 48 00 05 ]

bitbang_cmd(): [ 40 00 06 A0 ] [ E0 40 00 06 ]

bitbang_cmd(): [ 48 00 06 E0 ] [ A0 48 00 06 ]

bitbang_cmd(): [ 40 00 07 B1 ] [ E0 40 00 07 ]

bitbang_cmd(): [ 48 00 07 E0 ] [ B1 48 00 07 ]

#bitbang_cmd(): [ 40 00 08 01 ] [ E0 40 00 08 ]

bitbang_cmd(): [ 48 00 08 C0 ] [ 01 48 00 08 ]

bitbang_cmd(): [ 40 00 09 1D ] [ C0 40 00 09 ]

bitbang_cmd(): [ 48 00 09 92 ] [ 1D 48 00 09 ]

bitbang_cmd(): [ 40 00 0A A0 ] [ 92 40 00 0A ]

#bitbang_cmd(): [ 48 00 0A 30 ] [ A0 48 00 0A ]

bitbang_cmd(): [ 40 00 0B B1 ] [ 30 40 00 0B ]

bitbang_cmd(): [ 48 00 0B 07 ] [ B1 48 00 0B ]

bitbang_cmd(): [ 40 00 0C E1 ] [ 07 40 00 0C ]

bitbang_cmd(): [ 48 00 0C F7 ] [ E1 48 00 0C ]

#bitbang_cmd(): [ 40 00 0D 0E ] [ F7 40 00 0D ]

bitbang_cmd(): [ 48 00 0D 94 ] [ 0E 48 00 0D ]

bitbang_cmd(): [ 40 00 0E 67 ] [ 94 40 00 0E ]

bitbang_cmd(): [ 48 00 0E 00 ] [ 67 48 00 0E ]

bitbang_cmd(): [ 40 00 0F 0C ] [ 00 40 00 0F ]

#bitbang_cmd(): [ 48 00 0F 94 ] [ 0C 48 00 0F ]

bitbang_cmd(): [ 40 00 10 7A ] [ 94 40 00 10 ]

bitbang_cmd(): [ 48 00 10 00 ] [ 7A 48 00 10 ]

bitbang_cmd(): [ 40 00 11 0C ] [ 00 40 00 11 ]

bitbang_cmd(): [ 48 00 11 94 ] [ 0C 48 00 11 ]

#bitbang_cmd(): [ 40 00 12 00 ] [ 94 40 00 12 ]

bitbang_cmd(): [ 48 00 12 00 ] [ 00 48 00 12 ]

bitbang_cmd(): [ 40 00 13 8F ] [ 00 40 00 13 ]

bitbang_cmd(): [ 48 00 13 EF ] [ 8F 48 00 13 ]

bitbang_cmd(): [ 40 00 14 84 ] [ EF 40 00 14 ]

#bitbang_cmd(): [ 48 00 14 B9 ] [ 84 48 00 14 ]

bitbang_cmd(): [ 40 00 15 87 ] [ B9 40 00 15 ]

bitbang_cmd(): [ 48 00 15 B9 ] [ 87 48 00 15 ]

bitbang_cmd(): [ 40 00 16 8E ] [ B9 40 00 16 ]

bitbang_cmd(): [ 48 00 16 EF ] [ 8E 48 00 16 ]

#bitbang_cmd(): [ 40 00 17 8A ] [ EF 40 00 17 ]

bitbang_cmd(): [ 48 00 17 B9 ] [ 8A 48 00 17 ]

bitbang_cmd(): [ 40 00 18 08 ] [ B9 40 00 18 ]

bitbang_cmd(): [ 48 00 18 95 ] [ 08 48 00 18 ]

bitbang_cmd(): [ 40 00 19 0A ] [ 95 40 00 19 ]

#bitbang_cmd(): [ 48 00 19 C0 ] [ 0A 48 00 19 ]

bitbang_cmd(): [ 40 00 1A 2A ] [ C0 40 00 1A ]

bitbang_cmd(): [ 48 00 1A E5 ] [ 2A 48 00 1A ]

bitbang_cmd(): [ 40 00 1B 00 ] [ E5 40 00 1B ]

bitbang_cmd(): [ 48 00 1B 00 ] [ 00 48 00 1B ]

#bitbang_cmd(): [ 40 00 1C 00 ] [ 00 40 00 1C ]

bitbang_cmd(): [ 48 00 1C 00 ] [ 00 48 00 1C ]

bitbang_cmd(): [ 40 00 1D 00 ] [ 00 40 00 1D ]

bitbang_cmd(): [ 48 00 1D 00 ] [ 00 48 00 1D ]

bitbang_cmd(): [ 40 00 1E 00 ] [ 00 40 00 1E ]

#bitbang_cmd(): [ 48 00 1E 00 ] [ 00 48 00 1E ]

bitbang_cmd(): [ 40 00 1F 00 ] [ 00 40 00 1F ]

bitbang_cmd(): [ 48 00 1F 00 ] [ 00 48 00 1F ]

bitbang_cmd(): [ 40 00 20 00 ] [ 00 40 00 20 ]

bitbang_cmd(): [ 48 00 20 00 ] [ 00 48 00 20 ]

#bitbang_cmd(): [ 40 00 21 21 ] [ 00 40 00 21 ]

bitbang_cmd(): [ 48 00 21 50 ] [ 21 48 00 21 ]

bitbang_cmd(): [ 40 00 22 C1 ] [ 50 40 00 22 ]

bitbang_cmd(): [ 48 00 22 F7 ] [ C1 48 00 22 ]

bitbang_cmd(): [ 40 00 23 01 ] [ F7 40 00 23 ]

#bitbang_cmd(): [ 48 00 23 97 ] [ 01 48 00 23 ]

bitbang_cmd(): [ 40 00 24 00 ] [ 97 40 00 24 ]

bitbang_cmd(): [ 48 00 24 97 ] [ 00 48 00 24 ]

bitbang_cmd(): [ 40 00 25 A1 ] [ 97 40 00 25 ]

bitbang_cmd(): [ 48 00 25 F7 ] [ A1 48 00 25 ]

#bitbang_cmd(): [ 40 00 26 08 ] [ F7 40 00 26 ]

bitbang_cmd(): [ 48 00 26 95 ] [ 08 48 00 26 ]

bitbang_cmd(): [ 40 00 27 1F ] [ 95 40 00 27 ]

bitbang_cmd(): [ 48 00 27 93 ] [ 1F 48 00 27 ]

bitbang_cmd(): [ 40 00 28 0E ] [ 93 40 00 28 ]

#bitbang_cmd(): [ 48 00 28 94 ] [ 0E 48 00 28 ]

bitbang_cmd(): [ 40 00 29 53 ] [ 94 40 00 29 ]

bitbang_cmd(): [ 48 00 29 00 ] [ 53 48 00 29 ]

bitbang_cmd(): [ 40 00 2A 1F ] [ 00 40 00 2A ]

bitbang_cmd(): [ 48 00 2A EF ] [ 1F 48 00 2A ]

#bitbang_cmd(): [ 40 00 2B 18 ] [ EF 40 00 2B ]

bitbang_cmd(): [ 48 00 2B B9 ] [ 18 48 00 2B ]

bitbang_cmd(): [ 40 00 2C 15 ] [ B9 40 00 2C ]

bitbang_cmd(): [ 48 00 2C B9 ] [ 15 48 00 2C ]

bitbang_cmd(): [ 40 00 2D 1B ] [ B9 40 00 2D ]

#bitbang_cmd(): [ 48 00 2D B9 ] [ 1B 48 00 2D ]

bitbang_cmd(): [ 40 00 2E 84 ] [ B9 40 00 2E ]

bitbang_cmd(): [ 48 00 2E EF ] [ 84 48 00 2E ]

bitbang_cmd(): [ 40 00 2F 91 ] [ EF 40 00 2F ]

bitbang_cmd(): [ 48 00 2F E0 ] [ 91 48 00 2F ]

#bitbang_cmd(): [ 40 00 30 0E ] [ E0 40 00 30 ]

bitbang_cmd(): [ 48 00 30 94 ] [ 0E 48 00 30 ]

bitbang_cmd(): [ 40 00 31 59 ] [ 94 40 00 31 ]

bitbang_cmd(): [ 48 00 31 00 ] [ 59 48 00 31 ]

bitbang_cmd(): [ 40 00 32 18 ] [ 00 40 00 32 ]

#bitbang_cmd(): [ 48 00 32 B8 ] [ 18 48 00 32 ]

bitbang_cmd(): [ 40 00 33 15 ] [ B8 40 00 33 ]

bitbang_cmd(): [ 48 00 33 B8 ] [ 15 48 00 33 ]

bitbang_cmd(): [ 40 00 34 1B ] [ B8 40 00 34 ]

bitbang_cmd(): [ 48 00 34 B8 ] [ 1B 48 00 34 ]

#bitbang_cmd(): [ 40 00 35 84 ] [ B8 40 00 35 ]

bitbang_cmd(): [ 48 00 35 EF ] [ 84 48 00 35 ]

bitbang_cmd(): [ 40 00 36 91 ] [ EF 40 00 36 ]

bitbang_cmd(): [ 48 00 36 E0 ] [ 91 48 00 36 ]

bitbang_cmd(): [ 40 00 37 0E ] [ E0 40 00 37 ]

#bitbang_cmd(): [ 48 00 37 94 ] [ 0E 48 00 37 ]

bitbang_cmd(): [ 40 00 38 59 ] [ 94 40 00 38 ]

bitbang_cmd(): [ 48 00 38 00 ] [ 59 48 00 38 ]

bitbang_cmd(): [ 40 00 39 F1 ] [ 00 40 00 39 ]

bitbang_cmd(): [ 48 00 39 CF ] [ F1 48 00 39 ]

#bitbang_cmd(): [ 40 00 3A F8 ] [ CF 40 00 3A ]

bitbang_cmd(): [ 48 00 3A 94 ] [ F8 48 00 3A ]

bitbang_cmd(): [ 40 00 3B FF ] [ 94 40 00 3B ]

bitbang_cmd(): [ 48 00 3B CF ] [ FF 48 00 3B ]

bitbang_cmd(): [ 4C 00 40 00 ] [ CF 4C 00 40 ]

| 100% 0.10s

avrdude: 248 bytes of flash written

avrdude: verifying flash memory against blink_1MHz.hex:

avrdude: load data flash data from input file blink_1MHz.hex:

avrdude: input file blink_1MHz.hex auto detected as Intel Hex

avrdude: input file blink_1MHz.hex contains 248 bytes

avrdude: reading on-chip flash data:

Reading | bitbang_cmd(): [ 20 00 00 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 00 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 01 00 ] [ 00 20 00 34 ]

bitbang_cmd(): [ 28 00 01 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 02 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 02 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 03 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 03 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 04 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 04 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 05 00 ] [ 00 20 00 51 ]

#bitbang_cmd(): [ 28 00 05 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 06 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 06 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 07 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 07 00 ] [ 00 28 00 00 ]

#bitbang_cmd(): [ 20 00 08 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 08 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 09 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 09 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 0A 00 ] [ 00 20 00 0C ]

#bitbang_cmd(): [ 28 00 0A 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 0B 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 0B 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 0C 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 0C 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 0D 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 0D 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 0E 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 0E 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 0F 00 ] [ 00 20 00 51 ]

#bitbang_cmd(): [ 28 00 0F 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 10 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 10 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 11 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 11 00 ] [ 00 28 00 00 ]

#bitbang_cmd(): [ 20 00 12 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 12 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 13 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 13 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 14 00 ] [ 00 20 00 0C ]

#bitbang_cmd(): [ 28 00 14 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 15 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 15 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 16 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 16 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 17 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 17 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 18 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 18 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 19 00 ] [ 00 20 00 51 ]

#bitbang_cmd(): [ 28 00 19 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 1A 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 1A 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 1B 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 1B 00 ] [ 00 28 00 00 ]

#bitbang_cmd(): [ 20 00 1C 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 1C 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 1D 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 1D 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 1E 00 ] [ 00 20 00 0C ]

#bitbang_cmd(): [ 28 00 1E 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 1F 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 1F 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 20 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 20 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 21 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 21 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 22 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 22 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 23 00 ] [ 00 20 00 51 ]

#bitbang_cmd(): [ 28 00 23 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 24 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 24 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 25 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 25 00 ] [ 00 28 00 00 ]

#bitbang_cmd(): [ 20 00 26 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 26 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 27 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 27 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 28 00 ] [ 00 20 00 0C ]

#bitbang_cmd(): [ 28 00 28 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 29 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 29 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 2A 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 2A 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 2B 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 2B 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 2C 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 2C 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 2D 00 ] [ 00 20 00 51 ]

#bitbang_cmd(): [ 28 00 2D 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 2E 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 2E 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 2F 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 2F 00 ] [ 00 28 00 00 ]

#bitbang_cmd(): [ 20 00 30 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 30 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 31 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 31 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 32 00 ] [ 00 20 00 0C ]

#bitbang_cmd(): [ 28 00 32 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 33 00 ] [ 00 20 00 51 ]

bitbang_cmd(): [ 28 00 33 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 34 00 ] [ 00 20 00 11 ]

bitbang_cmd(): [ 28 00 34 00 ] [ 00 28 00 24 ]

#bitbang_cmd(): [ 20 00 35 00 ] [ 00 20 00 1F ]

bitbang_cmd(): [ 28 00 35 00 ] [ 00 28 00 BE ]

bitbang_cmd(): [ 20 00 36 00 ] [ 00 20 00 CF ]

bitbang_cmd(): [ 28 00 36 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 37 00 ] [ 00 20 00 D8 ]

#bitbang_cmd(): [ 28 00 37 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 38 00 ] [ 00 20 00 DE ]

bitbang_cmd(): [ 28 00 38 00 ] [ 00 28 00 BF ]

bitbang_cmd(): [ 20 00 39 00 ] [ 00 20 00 CD ]

bitbang_cmd(): [ 28 00 39 00 ] [ 00 28 00 BF ]

#bitbang_cmd(): [ 20 00 3A 00 ] [ 00 20 00 11 ]

bitbang_cmd(): [ 28 00 3A 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 3B 00 ] [ 00 20 00 A0 ]

bitbang_cmd(): [ 28 00 3B 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 3C 00 ] [ 00 20 00 B1 ]

#bitbang_cmd(): [ 28 00 3C 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 3D 00 ] [ 00 20 00 E8 ]

bitbang_cmd(): [ 28 00 3D 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 3E 00 ] [ 00 20 00 F0 ]

#bitbang_cmd(): [ 28 00 3E 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 3F 00 ] [ 00 20 00 02 ]

bitbang_cmd(): [ 28 00 3F 00 ] [ 00 28 00 C0 ]

bitbang_cmd(): [ 20 00 40 00 ] [ 00 20 00 05 ]

bitbang_cmd(): [ 28 00 40 00 ] [ 00 28 00 90 ]

#bitbang_cmd(): [ 20 00 41 00 ] [ 00 20 00 0D ]

bitbang_cmd(): [ 28 00 41 00 ] [ 00 28 00 92 ]

bitbang_cmd(): [ 20 00 42 00 ] [ 00 20 00 A0 ]

bitbang_cmd(): [ 28 00 42 00 ] [ 00 28 00 30 ]

bitbang_cmd(): [ 20 00 43 00 ] [ 00 20 00 B1 ]

#bitbang_cmd(): [ 28 00 43 00 ] [ 00 28 00 07 ]

bitbang_cmd(): [ 20 00 44 00 ] [ 00 20 00 D9 ]

bitbang_cmd(): [ 28 00 44 00 ] [ 00 28 00 F7 ]

bitbang_cmd(): [ 20 00 45 00 ] [ 00 20 00 11 ]

bitbang_cmd(): [ 28 00 45 00 ] [ 00 28 00 E0 ]

#bitbang_cmd(): [ 20 00 46 00 ] [ 00 20 00 A0 ]

bitbang_cmd(): [ 28 00 46 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 47 00 ] [ 00 20 00 B1 ]

bitbang_cmd(): [ 28 00 47 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 48 00 ] [ 00 20 00 01 ]

#bitbang_cmd(): [ 28 00 48 00 ] [ 00 28 00 C0 ]

bitbang_cmd(): [ 20 00 49 00 ] [ 00 20 00 1D ]

bitbang_cmd(): [ 28 00 49 00 ] [ 00 28 00 92 ]

bitbang_cmd(): [ 20 00 4A 00 ] [ 00 20 00 A0 ]

bitbang_cmd(): [ 28 00 4A 00 ] [ 00 28 00 30 ]

#bitbang_cmd(): [ 20 00 4B 00 ] [ 00 20 00 B1 ]

bitbang_cmd(): [ 28 00 4B 00 ] [ 00 28 00 07 ]

bitbang_cmd(): [ 20 00 4C 00 ] [ 00 20 00 E1 ]

bitbang_cmd(): [ 28 00 4C 00 ] [ 00 28 00 F7 ]

bitbang_cmd(): [ 20 00 4D 00 ] [ 00 20 00 0E ]

#bitbang_cmd(): [ 28 00 4D 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 4E 00 ] [ 00 20 00 67 ]

bitbang_cmd(): [ 28 00 4E 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 4F 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 4F 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 50 00 ] [ 00 20 00 7A ]

bitbang_cmd(): [ 28 00 50 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 51 00 ] [ 00 20 00 0C ]

bitbang_cmd(): [ 28 00 51 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 52 00 ] [ 00 20 00 00 ]

#bitbang_cmd(): [ 28 00 52 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 53 00 ] [ 00 20 00 8F ]

bitbang_cmd(): [ 28 00 53 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 54 00 ] [ 00 20 00 84 ]

bitbang_cmd(): [ 28 00 54 00 ] [ 00 28 00 B9 ]

#bitbang_cmd(): [ 20 00 55 00 ] [ 00 20 00 87 ]

bitbang_cmd(): [ 28 00 55 00 ] [ 00 28 00 B9 ]

bitbang_cmd(): [ 20 00 56 00 ] [ 00 20 00 8E ]

bitbang_cmd(): [ 28 00 56 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 57 00 ] [ 00 20 00 8A ]

#bitbang_cmd(): [ 28 00 57 00 ] [ 00 28 00 B9 ]

bitbang_cmd(): [ 20 00 58 00 ] [ 00 20 00 08 ]

bitbang_cmd(): [ 28 00 58 00 ] [ 00 28 00 95 ]

bitbang_cmd(): [ 20 00 59 00 ] [ 00 20 00 0A ]

bitbang_cmd(): [ 28 00 59 00 ] [ 00 28 00 C0 ]

#bitbang_cmd(): [ 20 00 5A 00 ] [ 00 20 00 2A ]

bitbang_cmd(): [ 28 00 5A 00 ] [ 00 28 00 E5 ]

bitbang_cmd(): [ 20 00 5B 00 ] [ 00 20 00 00 ]

bitbang_cmd(): [ 28 00 5B 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 5C 00 ] [ 00 20 00 00 ]

#bitbang_cmd(): [ 28 00 5C 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 5D 00 ] [ 00 20 00 00 ]

bitbang_cmd(): [ 28 00 5D 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 5E 00 ] [ 00 20 00 00 ]

bitbang_cmd(): [ 28 00 5E 00 ] [ 00 28 00 00 ]

#bitbang_cmd(): [ 20 00 5F 00 ] [ 00 20 00 00 ]

bitbang_cmd(): [ 28 00 5F 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 60 00 ] [ 00 20 00 00 ]

bitbang_cmd(): [ 28 00 60 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 61 00 ] [ 00 20 00 21 ]

#bitbang_cmd(): [ 28 00 61 00 ] [ 00 28 00 50 ]

bitbang_cmd(): [ 20 00 62 00 ] [ 00 20 00 C1 ]

bitbang_cmd(): [ 28 00 62 00 ] [ 00 28 00 F7 ]

bitbang_cmd(): [ 20 00 63 00 ] [ 00 20 00 01 ]

bitbang_cmd(): [ 28 00 63 00 ] [ 00 28 00 97 ]

#bitbang_cmd(): [ 20 00 64 00 ] [ 00 20 00 00 ]

bitbang_cmd(): [ 28 00 64 00 ] [ 00 28 00 97 ]

bitbang_cmd(): [ 20 00 65 00 ] [ 00 20 00 A1 ]

bitbang_cmd(): [ 28 00 65 00 ] [ 00 28 00 F7 ]

bitbang_cmd(): [ 20 00 66 00 ] [ 00 20 00 08 ]

#bitbang_cmd(): [ 28 00 66 00 ] [ 00 28 00 95 ]

bitbang_cmd(): [ 20 00 67 00 ] [ 00 20 00 1F ]

bitbang_cmd(): [ 28 00 67 00 ] [ 00 28 00 93 ]

bitbang_cmd(): [ 20 00 68 00 ] [ 00 20 00 0E ]

bitbang_cmd(): [ 28 00 68 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 69 00 ] [ 00 20 00 53 ]

bitbang_cmd(): [ 28 00 69 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 6A 00 ] [ 00 20 00 1F ]

bitbang_cmd(): [ 28 00 6A 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 6B 00 ] [ 00 20 00 18 ]

#bitbang_cmd(): [ 28 00 6B 00 ] [ 00 28 00 B9 ]

bitbang_cmd(): [ 20 00 6C 00 ] [ 00 20 00 15 ]

bitbang_cmd(): [ 28 00 6C 00 ] [ 00 28 00 B9 ]

bitbang_cmd(): [ 20 00 6D 00 ] [ 00 20 00 1B ]

bitbang_cmd(): [ 28 00 6D 00 ] [ 00 28 00 B9 ]

#bitbang_cmd(): [ 20 00 6E 00 ] [ 00 20 00 84 ]

bitbang_cmd(): [ 28 00 6E 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 6F 00 ] [ 00 20 00 91 ]

bitbang_cmd(): [ 28 00 6F 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 70 00 ] [ 00 20 00 0E ]

#bitbang_cmd(): [ 28 00 70 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 71 00 ] [ 00 20 00 59 ]

bitbang_cmd(): [ 28 00 71 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 72 00 ] [ 00 20 00 18 ]

bitbang_cmd(): [ 28 00 72 00 ] [ 00 28 00 B8 ]

#bitbang_cmd(): [ 20 00 73 00 ] [ 00 20 00 15 ]

bitbang_cmd(): [ 28 00 73 00 ] [ 00 28 00 B8 ]

bitbang_cmd(): [ 20 00 74 00 ] [ 00 20 00 1B ]

bitbang_cmd(): [ 28 00 74 00 ] [ 00 28 00 B8 ]

bitbang_cmd(): [ 20 00 75 00 ] [ 00 20 00 84 ]

#bitbang_cmd(): [ 28 00 75 00 ] [ 00 28 00 EF ]

bitbang_cmd(): [ 20 00 76 00 ] [ 00 20 00 91 ]

bitbang_cmd(): [ 28 00 76 00 ] [ 00 28 00 E0 ]

bitbang_cmd(): [ 20 00 77 00 ] [ 00 20 00 0E ]

bitbang_cmd(): [ 28 00 77 00 ] [ 00 28 00 94 ]

#bitbang_cmd(): [ 20 00 78 00 ] [ 00 20 00 59 ]

bitbang_cmd(): [ 28 00 78 00 ] [ 00 28 00 00 ]

bitbang_cmd(): [ 20 00 79 00 ] [ 00 20 00 F1 ]

bitbang_cmd(): [ 28 00 79 00 ] [ 00 28 00 CF ]

bitbang_cmd(): [ 20 00 7A 00 ] [ 00 20 00 F8 ]

#bitbang_cmd(): [ 28 00 7A 00 ] [ 00 28 00 94 ]

bitbang_cmd(): [ 20 00 7B 00 ] [ 00 20 00 FF ]

bitbang_cmd(): [ 28 00 7B 00 ] [ 00 28 00 CF ]

| 100% 0.08s

avrdude: verifying …

avrdude: 248 bytes of flash verified

bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]

bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]

bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]

avrdude: safemode: lfuse reads as 62

bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]

bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]

bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]

avrdude: safemode: hfuse reads as D9

bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]

bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]

bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]

avrdude: safemode: efuse reads as 7

avrdude: safemode: Fuses OK

avrdude done. Thank you.

Problem is that the LED still doesn’t blink. I tested the LEDs and they all seem to work independently of the controller.

Any help would be appreciated.

Thanks,

Chuck

How can you tell if the led is blinking or not? Surely no human can tell if a led is blinking at more than maybe 10-15 Hz… (and I doubt if the LED itself can turn on and off 1,000,000 times in a second)

It looks like you have successfully compiled your program and programmed the Arduino. It is likely that the Arduino is happily doing whatever your program is telling it to do. You have been too verbose with the output of avrdude, but if you need help with the program you may want to submit it for review.

Assuming that you’re using the blink_1MHz.c at http://www.sparkfun.com/tutorials/93 , that should work.

It appears from looking at your avrdude output that the MCU is programmed.

However how are you wiring up your ATmega328p? After programming, did you tie the reset line high with a 10k resistor?

jyoung:
Assuming that you’re using the blink_1MHz.c at http://www.sparkfun.com/tutorials/93 , that should work.

It appears from looking at your avrdude output that the MCU is programmed.

However how are you wiring up your ATmega328p? After programming, did you tie the reset line high with a 10k resistor?

Jyoung,

Yes it is the blink_1MHz from sparkfun tutorial.

Ok, so it looks like it is loaded correctly…Good. I am using the schematic from the tutorial, so the reset line “should” be high with a 10k. I guess I should take a look, and maybe just connect it directly to the 5v rail. Does it need a 10k resistor if I tie it directly to the 5v rail?

Thanks,

Chuck

Figured it out.

I left the programmer hooked up to the chip, and the reset line was connected to both the programmer and the 5v rail. Once I pulled the connection to the programmer everything worked fine. I found it because the voltage between the ground rail and the reset line while power was on was 0v, but between the reset line and the 5v rail I was getting a 5v reading. Power was going into the programmer instead of the chip.

Lessons learned :slight_smile:

Thanks for the help.

Chuck