Problem using Olimex-ARM-USB-OCD with OpenOCD in ubuntu 8.04

I am a newbie to linux and have the following setup:-

(1) Ubuntu 8.04

(2) libftd2xx.so.0.4.13

(3) OpenOCD svn 983

My problem is that when I connect my Olimex JTAG debugger and run the command openocd -f openocd.cfg I get the following message

Open On-Chip Debugger 1.0 (2008-10-09-01:58) svn:983
$URL: http://svn.berlios.de/svnroot/repos/openocd/trunk/src/openocd.c $
jtag_speed: 2
Error:  unable to open ftdi device: 2
Runtime error, file "command.c", line 436:

However when I run as root I get the following message

Open On-Chip Debugger 1.0 (2008-10-09-01:58) svn:983
$URL: http://svn.berlios.de/svnroot/repos/openocd/trunk/src/openocd.c $
jtag_speed: 2
Error:  JTAG communication failure, check connection, JTAG interface, target power etc.
Error:  trying to validate configured JTAG chain anyway...
Error:  Error validating JTAG scan chain, IR mismatch, scan returned 0x00
Error:  Could not validate JTAG chain, continuing anyway...
Warning:value captured during scan didn't pass the requested check: captured: 0x00 check_value: 0x01 check_mask: 0x0f
Warning:in_handler reported a failed check
Warning:value captured during scan didn't pass the requested check: captured: 0x00 check_value: 0x01 check_mask: 0x0f
Warning:in_handler reported a failed check
Warning:no telnet port specified, using default port 4444
Warning:no gdb port specified, using default port 3333
Warning:no tcl port specified, using default port 6666

Up until an hour before this post I never had to specify root to have the last data dump show.

Many thanks in advance.