Hi all!
I try to realize a webcam project. im going to control a selfmade webcam pan/tilt mount with my arduino.
I used the Skyduino sketch http://arduino.cc/blog/2010/02/17/skydu … e/?lang=es am it works really fine.
Now I want to switch on a bulb when “C” is pressed, so that the pan/tilt mount moves to the start-position and i have light to see whats going on in front of the cam. I tried to combine this with the skyduino sketch, but it doesn’t work ![]()
/*
======================================
SkyDuino Sketch - Hari Wiguna 2010
======================================
*/
#include <Servo.h>
#define RELAY_PIN 3
Servo xServo;
Servo yServo;
int stepSize = 10;
const int xInit = 90;
const int yInit = 90;
const int xMin = 0;
const int xMax = 180;
const int yMin = 0;
const int yMax = 180;
int x = xInit;
int y = yInit;
int xNew = x;
int yNew = y;
void setup()
{
Serial.begin(9600);
//establishContact(); // send a byte to establish contact until receiver responds
xServo.attach(5); // attaches the servo on pin 9 to the servo object
yServo.attach(6); // attaches the servo on pin 9 to the servo object
delay(1000);
MoveServo(xServo, xServo.read(), x);
MoveServo(yServo, yServo.read(), y);
delay(100);
pinMode(11, OUTPUT);
pinMode(RELAY_PIN, OUTPUT);
}
void loop()
{
static int relayVal = 0;
int cmd;
while (Serial.available() > 0)
{
cmd = Serial.read();
switch (cmd)
{
case 'C':
{
relayVal ^= 1; // xor current value with 1 (causes value to toggle)
if (relayVal)
Serial.println("Relay on");
else
Serial.println("Relay off");
break;
}
}
if (relayVal)
digitalWrite(RELAY_PIN, HIGH);
else
digitalWrite(RELAY_PIN, LOW);
}
// if we get a valid byte, read analog ins:
if (Serial.available() > 0) {
char msg = Serial.read();
if (msg == 'C') {xNew=xInit; yNew=yInit;}
if (msg == 'R') xNew = x - stepSize;
if (msg == 'L') xNew = x + stepSize;
if (msg == 'D') yNew = y - stepSize;
if (msg == 'U') yNew = y + stepSize;
xNew = constrain(xNew, xMin, xMax);
yNew = constrain(yNew, yMin, yMax);
}
MoveServo(xServo, x, xNew);
MoveServo(yServo, y, yNew);
x = xNew;
y = yNew;
}
void MoveServo(Servo servo, int moveFrom, int moveTo)
{
if (moveFrom <= moveTo)
{
for (int c=moveFrom; c<=moveTo; c++)
{
servo.write(c);
delay(50);
}
}
if (moveFrom > moveTo)
{
for (int c=moveFrom; c>=moveTo; c--)
{
servo.write(c);
delay(50);
}
}
}