Programming arduino uno

http://playground.arduino.cc/Code/AvailableMemory

… or comment out those arrays that won’t get used and see if your problem goes away.

The first step is to add debugging println’s at the beginning and end of every logic break (loops, functions, etc…) and for the values of the variables involved. That will tell you what is happening. LED’s being on and off don’t tell you that. This should make it apparent exactly where your problem is.

The gsm module is just another serial connection. I can’t see it having anything to do with this at all unless you are powering the gsm with your primary power source or you have not connected all of your ground wires together.

Mee_n_Mac:
http://playground.arduino.cc/Code/AvailableMemory

… or comment out those arrays that won’t get used and see if your problem goes away.

Sir, I used this function for memory test (sram space left in bytes)

int freeRam () {
  extern int __heap_start, *__brkval; 
  int v; 
  return (int) &v - (__brkval == 0 ? (int) &__heap_start : (int) __brkval); 
}

and call it anywhere in your program like that: Serial.println(freeRam());

But, it shows at various points that I defined in the code, that free space is 1388. So , I do not think it is an SRAM problem. What do you think??

These are the various points at which I used it.

void policeLights() {
digitalWrite(blue, HIGH);
[size=150]Serial.println(freeRam())[/size]; 
cell.println("AT+CMGF=1"); // set SMS mode to text
cell.print("AT+CMGS=");  // now send message...[size=150][/size]
cell.write((byte)34);  // ASCII equivalent of "
cell.print(mobilenumber);
cell.write((byte)34);   // ASCII equivalent of "
cell.println();
delay(500); // give the module some thinking time
cell.print("hi bobby, the king of kings... :-)");   // our message to send
cell.write((byte)26); // ASCII equivalent of Ctrl-Z
cell.println();
[size=150]Serial.println(freeRam()); [/size]
delay(15000); // the SMS module needs time to return to OK status
[size=150]Serial.println(freeRam()); [/size]
}
void setup() {
  Serial.begin(9600);
  setupSpeedZones();
  [size=150]Serial.println(freeRam()); [/size]
  blue = 12;
  pinMode(blue, OUTPUT);
  pinMode(TEST_BUTTON, INPUT);
  digitalWrite(TEST_BUTTON, HIGH);
void setupSpeedZones() {
 [size=150]Serial.println(freeRam()); [/size]

speedZones[0] = &SpeedZone(10);
speedZones[0]->setVertices(10, (Vertex[10]){
Vertex(12.938231,77.533291),
Vertex(12.937279,77.533835),
Vertex(12.936665,77.534077),
Vertex(12.93524,77.536153),
Vertex(12.933635,77.538924),
Vertex(12.934012,77.53902),
Vertex(12.935515,77.536367),
Vertex(12.936756,77.534332),
Vertex(12.937342,77.53412),
Vertex(12.938456,77.533546)});
.
.
.
.
.
.
.
speedZones[4] = &SpeedZone(10);
speedZones[4]->setVertices(4, (Vertex[4]){
Vertex(12.935193,77.535496),
Vertex(12.933238,77.535635),
Vertex(12.933165,77.534283),
Vertex(12.935219,77.534155)});

[size=150]Serial.println(freeRam()); [/size]

for all these I got the same result of 1388 or similar.

I think it has got something to do with gsm program part, and arduino receiving a response from gsm. Please help.

What do the other print statements I suggested back on page 1 show for the state or “speeding” or “buttonPressed” when the bad stuff happens ?

I don’t have the GSM or GPS attached so I commented out the reads from the GPS. I added some prints to the loop() and I don’t see any hangup on my Arduino. The loop runs and policelights() is called and returned from. I see the kind of cyclic behavior I would expect.

This is “commented out” code I used. Button pressed was hard coded to be true.

#include <SoftwareSerial.h>
#include <TinyGPS.h>

#define NUM_OFF 2
#define DELAY 50
#define TEST_BUTTON 9
#define DEFAULT_SPEED_LIMIT 5
#define NSPEEDZONES 6

boolean debugMode = true;

boolean speeding = false;
int blue;
int loopctr = 0;



class Vertex {
public:
  Vertex(float llat, float llng) {
    lat = llat;
    lng = llng;
  }
  float lat;
  float lng;
};

class SpeedZone {
public:
  SpeedZone(int s) {
    speedLimit = s;
  }
  void setVertices(int n, Vertex *v) {
    nVertices = n;
    vertices = v;
  }
  int nVertices;
  Vertex *vertices;
  int speedLimit;
};


SpeedZone *speedZones[NSPEEDZONES];
//TinyGPS gps;
SoftwareSerial nss(3, 4);
boolean buttonPressed = false;
SoftwareSerial cell(7,8);  // We need to create a serial port on D2/D3 to talk to the GSM module
char mobilenumber[] = "XXXXXXXXXXX"; 


void setup() {
  Serial.begin(9600);
  setupSpeedZones();
  blue = 12;
  pinMode(blue, OUTPUT);
  pinMode(TEST_BUTTON, INPUT);
  digitalWrite(TEST_BUTTON, HIGH);
  cell.begin(4800);
  delay(3500); // give the GSM module time to initialise, locate network etc.



  delay(3000);


  nss.begin(9600);
}



void setupSpeedZones() {

  // 2nd main road
  speedZones[0] = &SpeedZone(25);
  speedZones[0]->setVertices(12, (Vertex[12]){
    Vertex(12.943427649396137, 77.53860712051392),
    Vertex(12.942570236686135, 77.53871440887451),
    Vertex(12.94140958795451,77.53876805305481),
    Vertex(12.940980878498074, 77.53875732421875),
    Vertex(12.940353497477103, 77.5388753414154),
    Vertex(12.939046448613755,77.5390899181366 ),
    Vertex(12.938021717514202,77.53932595252991 ),
    Vertex(12.937760305845364,77.53974437713623 ),
    Vertex(12.93687150412194,77.53973364830017 ),
    Vertex(12.935982699231385,77.53956198692322 ),
    Vertex(12.934142340214253,77.53906846046448),
    Vertex(12.933943664281175,77.538982629776 )  }
  );


  // 80 feet Double Road
  speedZones[1] = &SpeedZone(15);
  speedZones[1]->setVertices(9, (Vertex[9]){
    Vertex(12.941044923555157, 77.53885790705681),
    Vertex(12.941039695387857, 77.53906175494194),
    Vertex(12.941035774262303, 77.5392173230648),
    Vertex(12.941027932011004, 77.53935679793358),
    Vertex(12.940876315104193, 77.54202961921692),
    Vertex(12.94081357704682, 77.54283428192139),
    Vertex(12.940698557233977, 77.54501223564148),
    Vertex(12.94058353736807,77.54695415496826 ),
    Vertex(12.940520799237047, 77.54763007164001)  }
  );



  //  Block road
  speedZones[2] = &SpeedZone(10);
  speedZones[2]->setVertices(16, (Vertex[16]){
    Vertex(12.933547619021462,77.53549307584763),
    Vertex(12.93361689431027,77.53550313413143 ),
    Vertex(12.933661988591705,77.5354977697134),
    Vertex(12.933694012061984,77.53548838198185),
    Vertex(12.933777665189446,77.53545552492142),
    Vertex(12.933820798822312,77.5354354083538),
    Vertex(12.933860664749114,77.53541797399521),
    Vertex(12.934049537659947,77.53533147275448),
    Vertex(12.93419985163906,77.53525167703629),
    Vertex(12.934398527368137,77.53516852855682),
    Vertex(12.934513550086338,77.53511488437653),
    Vertex(12.934594588787776,77.53507733345032),
    Vertex(12.93473575291451,77.53501027822495),
    Vertex(12.934853389625761,77.53495931625366),
    Vertex(12.934952727249843,77.5349110364914),
    Vertex(12.934984097017653,77.53490567207336)  }
  );



  // towards  post office
  speedZones[3] = &SpeedZone(35);
  speedZones[3]->setVertices(20, (Vertex[20]){
    Vertex(12.93382341298164, 77.53911674022675),
    Vertex(12.933729303228546, 77.53927633166313),
    Vertex(12.933663949212452, 77.53939434885979),
    Vertex(12.933615587229529, 77.5394868850708),
    Vertex(12.933513634910476,77.53962635993958 ),
    Vertex(12.9334495879195, 77.5397376716137),
    Vertex(12.933313651394398, 77.53990530967712),
    Vertex(12.933197321040067, 77.54006892442703),
    Vertex(12.933090140216153, 77.54023790359497),
    Vertex(12.933005179774247, 77.54036530852318),
    Vertex(12.932905841374719, 77.54049941897392),
    Vertex(12.932785589574985,  77.54066303372383),
    Vertex(12.932637888915574, 77.54087224602699),
    Vertex(12.932517636986722, 77.54102379083633),
    Vertex(12.932401306261246, 77.54119008779526),
    Vertex(12.932307195971756, 77.54131078720093),
    Vertex(12.932219621087134, 77.54143953323364),
    Vertex(12.932149038321938, 77.54154548048973),
    Vertex(12.93218171553054, 77.54162460565567),
    Vertex(12.932209164382444, 77.54164338111877)  }
  );


  // ring road
  speedZones[4] = &SpeedZone(40);
  speedZones[4]->setVertices(11, (Vertex[11]){
    Vertex(12.933744988189858, 77.53884315490723),
    Vertex(12.93417371008398, 77.53815650939941),
    Vertex(12.934696540665088, 77.53731966018677),
    Vertex(12.935062521419919, 77.53671884536743),
    Vertex(12.935313479341485, 77.53631114959717),
    Vertex(12.935648089510861, 77.53558158874512),
    Vertex(12.936087264677003, 77.53476619720459),
    Vertex(12.936599634726921, 77.53420829772949),
    Vertex(12.937321133624925, 77.53389716148376),
    Vertex(12.937948522274533, 77.53362894058228),
    Vertex(12.938230846651972, 77.53344655036926)  }
  );



  // new road
  speedZones[5] = &SpeedZone(30);
  speedZones[5]->setVertices(11, (Vertex[11]){
    Vertex(12.943443333747508, 77.5386044383049),
    Vertex(12.943435491571943, 77.53841936588287),
    Vertex(12.943432877513375, 77.53809481859207),
    Vertex(12.943432877513375, 77.53791779279709),
    Vertex(12.943425035337478, 77.53762006759644),
    Vertex(12.943417193161341, 77.53743767738342),
    Vertex(12.943409350984949, 77.53721237182617),
    Vertex(12.943411965043772, 77.53708630800247),
    Vertex(12.943406736926102, 77.53692269325256),
    Vertex(12.94338582445431, 77.53680735826492),
    Vertex(12.943357069802731, 77.53675907850266)  }
  );


  if (debugMode) {
    printSpeedZones();
  }

}


boolean inSpeedZone(int speedZone, float lat, float lng) {
  SpeedZone *s = speedZones[speedZone];

  int i, j;
  boolean inside = false;
  for (i = 0, j = s->nVertices-1; i < s->nVertices; j = i++) {
    if ( ((s->vertices[i].lat > lat) != (s->vertices[j].lat > lat)) &&
      (lng < (s->vertices[j].lng - s->vertices[i].lng) * (lat - s->vertices[i].lat) / (s->vertices[j].lat - s->vertices[i].lat) + s->vertices[i].lng) )
      inside = !inside;
  }

  return inside;
}


boolean inSpeedZone(int speedZone) {
  float lat, lng;
  unsigned long  fix_age;

  // retrieves +/- lat/long in 100,000ths of a degree
  //gps.f_get_position(&lat, &lng, &fix_age);

  return inSpeedZone(speedZone, lat, lng);
}

void loop() {
  loopctr++;
  Serial.print("Loop counter  = ");
  Serial.println(loopctr);
//  if (readGPS()) {
//    if (debugMode) {
//      debug();
//    }
//    speeding = isSpeeding();
//  }

//  if (digitalRead(TEST_BUTTON) == LOW) {
//    buttonPressed = true;
//  } 
//  else {
//    buttonPressed = false;
//  }
  buttonPressed = true;
  if ((speeding || buttonPressed) && (!(speeding && buttonPressed))) {
    Serial.println("going to PD lights");
    policeLights();
  } 
  else {
    allOff();
  }

}

//bool readGPS() {
//  while (nss.available()) {
//    if (gps.encode(nss.read())) {
//      return true;
//    }
//  }
//  return false;
//}


int getSpeedLimit() {
  boolean isInSpeedZone;

  for(int i=0;i<NSPEEDZONES;i++) {
    isInSpeedZone = inSpeedZone(i);
    if (isInSpeedZone) {
      return speedZones[i]->speedLimit;
    }
  }
  return DEFAULT_SPEED_LIMIT;
}

//boolean isSpeeding() {
//  int speed = (int)(gps.f_speed_kmph() + 0.5);
//  int speedLimit = getSpeedLimit();

//  if (speed > speedLimit) {
//    delay (5000);
//    if (speed > speedLimit)
//      return true;
//  }
//  return false;
//}

void policeLights() {
  Serial.println("In PD lights");
  digitalWrite(blue, HIGH);
  cell.println("AT+CMGF=1"); // set SMS mode to text
  cell.print("AT+CMGS=");  // now send message...
  cell.write((byte)34);  // ASCII equivalent of "
  cell.print(mobilenumber);
  cell.write((byte)34);   // ASCII equivalent of "
  cell.println();
  delay(500); // give the module some thinking time
  cell.print("hi bobby, the king of kings... :-)");   // our message to send
  cell.write((byte)26); // ASCII equivalent of Ctrl-Z
  cell.println();
  delay(15000); // the SMS module needs time to return to OK status
  Serial.println("Exit PD lights");
  return;
}


void allOff() {
  digitalWrite(blue,LOW);
}

void printSpeedZones() {

  for(int i=0;i<NSPEEDZONES;i++) {
    SpeedZone *s = speedZones[i];
    Serial.println(s->speedLimit);
    for(int v=0;v<s->nVertices;v++) {
      Serial.print("(");
      Serial.print(s->vertices[v].lat,15);
      Serial.print(", ");
      Serial.print(s->vertices[v].lng,15);
      Serial.println(")");
    }
  }
}

void debug() {
  float lat, lng;
  unsigned long fix_age, time, date, speed, course;

  // retrieves +/- lat/long in 100000ths of a degree
  //gps.f.get_position(&lat, &lng, &fix_age);

  Serial.println(getSpeedLimit());

  Serial.print("lat: ");
  Serial.print(lat,15);
  Serial.print("    lng: ");
  Serial.print(lng,15);
  Serial.print("    speed: ");
  //Serial.println(gps.f_speed_kmph());
}

And this is the looping behavior I see :

Loop counter = 1

going to PD lights

In PD lights

Exit PD lights

Loop counter = 2

going to PD lights

In PD lights

Exit PD lights

Loop counter = 3

going to PD lights

In PD lights

Exit PD lights

Loop counter = 4

going to PD lights

In PD lights

Exit PD lights

Loop counter = 5

going to PD lights

In PD lights

Exit PD lights

Loop counter = 6

going to PD lights

In PD lights

Exit PD lights

Loop counter = 7

going to PD lights

In PD lights

Exit PD lights

Loop counter = 8

going to PD lights

In PD lights

Exit PD lights

Loop counter = 9

going to PD lights

In PD lights

Exit PD lights

Loop counter = 10

going to PD lights

In PD lights

Exit PD lights

Loop counter = 11

going to PD lights

In PD lights

Exit PD lights

Loop counter = 12

going to PD lights

In PD lights

Exit PD lights

Loop counter = 13

going to PD lights

In PD lights

Exit PD lights

Loop counter = 14

going to PD lights

In PD lights

Exit PD lights

Loop counter = 15

going to PD lights

In PD lights

Exit PD lights

Loop counter = 16

going to PD lights

In PD lights

Exit PD lights

Mee_n_Mac:
This is “commented out” code I used. Button pressed was hard coded to be true.

#include <SoftwareSerial.h>

#include <TinyGPS.h>

#define NUM_OFF 2
#define DELAY 50
#define TEST_BUTTON 9
#define DEFAULT_SPEED_LIMIT 5
#define NSPEEDZONES 6

boolean debugMode = true;

boolean speeding = false;
int blue;
int loopctr = 0;

class Vertex {
public:
Vertex(float llat, float llng) {
lat = llat;
lng = llng;
}
float lat;
float lng;
};

class SpeedZone {
public:
SpeedZone(int s) {
speedLimit = s;
}
void setVertices(int n, Vertex *v) {
nVertices = n;
vertices = v;
}
int nVertices;
Vertex *vertices;
int speedLimit;
};

SpeedZone *speedZones[NSPEEDZONES];
//TinyGPS gps;
SoftwareSerial nss(3, 4);
boolean buttonPressed = false;
SoftwareSerial cell(7,8); // We need to create a serial port on D2/D3 to talk to the GSM module
char mobilenumber = “XXXXXXXXXXX”;

void setup() {
Serial.begin(9600);
setupSpeedZones();
blue = 12;
pinMode(blue, OUTPUT);
pinMode(TEST_BUTTON, INPUT);
digitalWrite(TEST_BUTTON, HIGH);
cell.begin(4800);
delay(3500); // give the GSM module time to initialise, locate network etc.

delay(3000);

nss.begin(9600);
}

void setupSpeedZones() {

// 2nd main road
speedZones[0] = &SpeedZone(25);
speedZones[0]->setVertices(12, (Vertex[12]){
Vertex(12.943427649396137, 77.53860712051392),
Vertex(12.942570236686135, 77.53871440887451),
Vertex(12.94140958795451,77.53876805305481),
Vertex(12.940980878498074, 77.53875732421875),
Vertex(12.940353497477103, 77.5388753414154),
Vertex(12.939046448613755,77.5390899181366 ),
Vertex(12.938021717514202,77.53932595252991 ),
Vertex(12.937760305845364,77.53974437713623 ),
Vertex(12.93687150412194,77.53973364830017 ),
Vertex(12.935982699231385,77.53956198692322 ),
Vertex(12.934142340214253,77.53906846046448),
Vertex(12.933943664281175,77.538982629776 ) }
);

// 80 feet Double Road
speedZones[1] = &SpeedZone(15);
speedZones[1]->setVertices(9, (Vertex[9]){
Vertex(12.941044923555157, 77.53885790705681),
Vertex(12.941039695387857, 77.53906175494194),
Vertex(12.941035774262303, 77.5392173230648),
Vertex(12.941027932011004, 77.53935679793358),
Vertex(12.940876315104193, 77.54202961921692),
Vertex(12.94081357704682, 77.54283428192139),
Vertex(12.940698557233977, 77.54501223564148),
Vertex(12.94058353736807,77.54695415496826 ),
Vertex(12.940520799237047, 77.54763007164001) }
);

// Block road
speedZones[2] = &SpeedZone(10);
speedZones[2]->setVertices(16, (Vertex[16]){
Vertex(12.933547619021462,77.53549307584763),
Vertex(12.93361689431027,77.53550313413143 ),
Vertex(12.933661988591705,77.5354977697134),
Vertex(12.933694012061984,77.53548838198185),
Vertex(12.933777665189446,77.53545552492142),
Vertex(12.933820798822312,77.5354354083538),
Vertex(12.933860664749114,77.53541797399521),
Vertex(12.934049537659947,77.53533147275448),
Vertex(12.93419985163906,77.53525167703629),
Vertex(12.934398527368137,77.53516852855682),
Vertex(12.934513550086338,77.53511488437653),
Vertex(12.934594588787776,77.53507733345032),
Vertex(12.93473575291451,77.53501027822495),
Vertex(12.934853389625761,77.53495931625366),
Vertex(12.934952727249843,77.5349110364914),
Vertex(12.934984097017653,77.53490567207336) }
);

// towards post office
speedZones[3] = &SpeedZone(35);
speedZones[3]->setVertices(20, (Vertex[20]){
Vertex(12.93382341298164, 77.53911674022675),
Vertex(12.933729303228546, 77.53927633166313),
Vertex(12.933663949212452, 77.53939434885979),
Vertex(12.933615587229529, 77.5394868850708),
Vertex(12.933513634910476,77.53962635993958 ),
Vertex(12.9334495879195, 77.5397376716137),
Vertex(12.933313651394398, 77.53990530967712),
Vertex(12.933197321040067, 77.54006892442703),
Vertex(12.933090140216153, 77.54023790359497),
Vertex(12.933005179774247, 77.54036530852318),
Vertex(12.932905841374719, 77.54049941897392),
Vertex(12.932785589574985, 77.54066303372383),
Vertex(12.932637888915574, 77.54087224602699),
Vertex(12.932517636986722, 77.54102379083633),
Vertex(12.932401306261246, 77.54119008779526),
Vertex(12.932307195971756, 77.54131078720093),
Vertex(12.932219621087134, 77.54143953323364),
Vertex(12.932149038321938, 77.54154548048973),
Vertex(12.93218171553054, 77.54162460565567),
Vertex(12.932209164382444, 77.54164338111877) }
);

// ring road
speedZones[4] = &SpeedZone(40);
speedZones[4]->setVertices(11, (Vertex[11]){
Vertex(12.933744988189858, 77.53884315490723),
Vertex(12.93417371008398, 77.53815650939941),
Vertex(12.934696540665088, 77.53731966018677),
Vertex(12.935062521419919, 77.53671884536743),
Vertex(12.935313479341485, 77.53631114959717),
Vertex(12.935648089510861, 77.53558158874512),
Vertex(12.936087264677003, 77.53476619720459),
Vertex(12.936599634726921, 77.53420829772949),
Vertex(12.937321133624925, 77.53389716148376),
Vertex(12.937948522274533, 77.53362894058228),
Vertex(12.938230846651972, 77.53344655036926) }
);

// new road
speedZones[5] = &SpeedZone(30);
speedZones[5]->setVertices(11, (Vertex[11]){
Vertex(12.943443333747508, 77.5386044383049),
Vertex(12.943435491571943, 77.53841936588287),
Vertex(12.943432877513375, 77.53809481859207),
Vertex(12.943432877513375, 77.53791779279709),
Vertex(12.943425035337478, 77.53762006759644),
Vertex(12.943417193161341, 77.53743767738342),
Vertex(12.943409350984949, 77.53721237182617),
Vertex(12.943411965043772, 77.53708630800247),
Vertex(12.943406736926102, 77.53692269325256),
Vertex(12.94338582445431, 77.53680735826492),
Vertex(12.943357069802731, 77.53675907850266) }
);

if (debugMode) {
printSpeedZones();
}

}

boolean inSpeedZone(int speedZone, float lat, float lng) {
SpeedZone *s = speedZones[speedZone];

int i, j;
boolean inside = false;
for (i = 0, j = s->nVertices-1; i < s->nVertices; j = i++) {
if ( ((s->vertices[i].lat > lat) != (s->vertices[j].lat > lat)) &&
(lng < (s->vertices[j].lng - s->vertices[i].lng) * (lat - s->vertices[i].lat) / (s->vertices[j].lat - s->vertices[i].lat) + s->vertices[i].lng) )
inside = !inside;
}

return inside;
}

boolean inSpeedZone(int speedZone) {
float lat, lng;
unsigned long fix_age;

// retrieves +/- lat/long in 100,000ths of a degree
//gps.f_get_position(&lat, &lng, &fix_age);

return inSpeedZone(speedZone, lat, lng);
}

void loop() {
loopctr++;
Serial.print("Loop counter = ");
Serial.println(loopctr);
// if (readGPS()) {
// if (debugMode) {
// debug();
// }
// speeding = isSpeeding();
// }

// if (digitalRead(TEST_BUTTON) == LOW) {
// buttonPressed = true;
// }
// else {
// buttonPressed = false;
// }
buttonPressed = true;
if ((speeding || buttonPressed) && (!(speeding && buttonPressed))) {
Serial.println(“going to PD lights”);
policeLights();
}
else {
allOff();
}

}

//bool readGPS() {
// while (nss.available()) {
// if (gps.encode(nss.read())) {
// return true;
// }
// }
// return false;
//}

int getSpeedLimit() {
boolean isInSpeedZone;

for(int i=0;i<NSPEEDZONES;i++) {
isInSpeedZone = inSpeedZone(i);
if (isInSpeedZone) {
return speedZones[i]->speedLimit;
}
}
return DEFAULT_SPEED_LIMIT;
}

//boolean isSpeeding() {
// int speed = (int)(gps.f_speed_kmph() + 0.5);
// int speedLimit = getSpeedLimit();

// if (speed > speedLimit) {
// delay (5000);
// if (speed > speedLimit)
// return true;
// }
// return false;
//}

void policeLights() {
Serial.println(“In PD lights”);
digitalWrite(blue, HIGH);
cell.println(“AT+CMGF=1”); // set SMS mode to text
cell.print(“AT+CMGS=”); // now send message…
cell.write((byte)34); // ASCII equivalent of "
cell.print(mobilenumber);
cell.write((byte)34); // ASCII equivalent of "
cell.println();
delay(500); // give the module some thinking time
cell.print(“hi bobby, the king of kings… :-)”); // our message to send
cell.write((byte)26); // ASCII equivalent of Ctrl-Z
cell.println();
delay(15000); // the SMS module needs time to return to OK status
Serial.println(“Exit PD lights”);
return;
}

void allOff() {
digitalWrite(blue,LOW);
}

void printSpeedZones() {

for(int i=0;i<NSPEEDZONES;i++) {
SpeedZone *s = speedZones[i];
Serial.println(s->speedLimit);
for(int v=0;vnVertices;v++) {
Serial.print(“(”);
Serial.print(s->vertices[v].lat,15);
Serial.print(“, “);
Serial.print(s->vertices[v].lng,15);
Serial.println(”)”);
}
}
}

void debug() {
float lat, lng;
unsigned long fix_age, time, date, speed, course;

// retrieves +/- lat/long in 100000ths of a degree
//gps.f.get_position(&lat, &lng, &fix_age);

Serial.println(getSpeedLimit());

Serial.print("lat: “);
Serial.print(lat,15);
Serial.print(” lng: “);
Serial.print(lng,15);
Serial.print(” speed: ");
//Serial.println(gps.f_speed_kmph());
}




And this is the looping behavior I see :
<QUOTE>

> Loop counter = 1
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 2
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 3
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 4
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 5
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 6
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 7
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 8
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 9
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 10
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 11
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 12
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 13
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 14
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 15
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights
> 
> Loop counter = 16
> 
> going to PD lights
> 
> In PD lights
> 
> Exit PD lights

</QUOTE>

This worked for me also, but with both the gsm and gps modules it fails. (the arduino cannot receive data simultaneously from gps and gsm I guess)

So, I used another arduino uno board for gsm module, such that a message is sent when a certain pin is activated on the second arduino, by a pin on the 1st arduino. This one worked properly without any hitches so far.

Now, I need to send the lat and long values of the place where the speeding condition has occurred, through the gsm module to a mobile phone.

Is it possible? How to do this?

This is because, the coordinates on the 1st arduino needs to be sent to 2nd arduino, and then to the mobile phone through gsm.

bobxcool:
…(the arduino cannot receive data simultaneously from gps and gsm I guess)…

These are just serial devices, no different than the connection to your computer through Serial. There is no software reason the gps and gsm cannot both be connected. If you power them both from your uno, you may run into problems with not providing enough power causing brownouts and reseting. If you don’t connect the grounds from the power sources of all devices connected to you uno you may run into other interesting and potentially magic smoke releasing problems. But, the uno is quite capable of handling many serial connections.

Post the output of the debug printlns and describe how the gps and gsm are powered and connected to the uno and we’ll help you get to a working project.

WethaGuy:

bobxcool:
…(the arduino cannot receive data simultaneously from gps and gsm I guess)…

These are just serial devices, no different than the connection to your computer through Serial. There is no software reason the gps and gsm cannot both be connected.

Post the output of the debug printlns and describe how the gps and gsm are powered and connected to the uno and we’ll help you get to a working project.

FWIW : I see he’s using software emulation of a UART to communicate with the GSM and GPS. From the page …

http://arduino.cc/en/Reference/SoftwareSerial

Limitations
The library has the following known limitations:
* If using multiple software serial ports, only one can receive data at a time.

I hadn’t seen where the GPS and GSM were both talking at the same time but I suppose the GPS is just spewing out NMEA messages constantly so overlap can happen. I believe you can tell most GPS’s to stop transmission so that would be a preferable alternative to using another Uno. I don’t know how to disable just one ‘port’ or it’s interrupts, but that would be another way.

I’d still like to see the prints of what’s happening with buttonPressed and speeding, then again maybe not. I’ve completely lost track of what the OP is running for code at this point. I did look briefly at the amount of variables involved at storing all the vertices and it’s under 1k, so the reported SRAM usage seem right and not a problem. I will point out that the accuracy available (as previously noted) doesn’t support the number of digits used.

http://arduino.cc/en/Reference/Float

Datatype for floating-point numbers, a number that has a decimal point. Floating-point numbers are often used to approximate analog and continuous values because they have greater resolution than integers. Floating-point numbers can be as large as 3.4028235E+38 and as low as -3.4028235E+38. They are stored as 32 bits (4 bytes) of information.
Floats have only 6-7 decimal digits of precision. That means the total number of digits, not the number to the right of the decimal point. Unlike other platforms, where you can get more precision by using a double (e.g. up to 15 digits), on the Arduino, double is the same size as float.

bobxcool:
Now, I need to send the lat and long values of the place where the speeding condition has occurred, through the gsm module to a mobile phone.

Is it possible? How to do this?

This is because, the coordinates on the 1st arduino needs to be sent to 2nd arduino, and then to the mobile phone through gsm.

I don't understand. Isn't this why you have a serial link __*to*__ the GSM ? I can't say I know much about it but I thought you could set up the GSM via some command codes and then just send the data. It would be ASCII text for for SMS and, I assume ( :o ) "raw data" for other modes. A cell.print and a cell.write respectively.

Mee_n_Mac:

WethaGuy:

bobxcool:
…(the arduino cannot receive data simultaneously from gps and gsm I guess)…

These are just serial devices, no different than the connection to your computer through Serial. There is no software reason the gps and gsm cannot both be connected.

Post the output of the debug printlns and describe how the gps and gsm are powered and connected to the uno and we’ll help you get to a working project.

FWIW : I see he’s using software emulation of a UART to communicate with the GSM and GPS. From the page …

http://arduino.cc/en/Reference/SoftwareSerial

Limitations
The library has the following known limitations:
* If using multiple software serial ports, only one can receive data at a time.

I hadn’t seen where the GPS and GSM were both talking at the same time but I suppose the GPS is just spewing out NMEA messages constantly so overlap can happen. I believe you can tell most GPS’s to stop transmission so that would be a preferable alternative to using another Uno. I don’t know how to disable just one ‘port’ or it’s interrupts, but that would be another way.

I’d still like to see the prints of what’s happening with buttonPressed and speeding, then again maybe not. I’ve completely lost track of what the OP is running for code at this point. I did look briefly at the amount of variables involved at storing all the vertices and it’s under 1k, so the reported SRAM usage seem right and not a problem. I will point out that the accuracy available (as previously noted) doesn’t support the number of digits used.

http://arduino.cc/en/Reference/Float

Datatype for floating-point numbers, a number that has a decimal point. Floating-point numbers are often used to approximate analog and continuous values because they have greater resolution than integers. Floating-point numbers can be as large as 3.4028235E+38 and as low as -3.4028235E+38. They are stored as 32 bits (4 bytes) of information.
Floats have only 6-7 decimal digits of precision. That means the total number of digits, not the number to the right of the decimal point. Unlike other platforms, where you can get more precision by using a double (e.g. up to 15 digits), on the Arduino, double is the same size as float.

sir, I tried to stop gps data transmission when gsm is working and vice-versa. but still the problem persists.

#include <SoftwareSerial.h>
#include <TinyGPS.h>

#define NUM_OFF 2
#define DELAY 50
#define DEFAULT_SPEED_LIMIT 50
#define NSPEEDZONES 5

boolean debugMode = true;

boolean speeding = false;
int blue;
int red;



class Vertex {
public:
  Vertex(float llat, float llng) {
    lat = llat;
    lng = llng;
  }
  float lat;
  float lng;
};

class SpeedZone {
public:
  SpeedZone(int s) {
    speedLimit = s;
  }
  void setVertices(int n, Vertex *v) {
    nVertices = n;
    vertices = v;
  }
  int nVertices;
  Vertex *vertices;
  int speedLimit;
};


SpeedZone *speedZones[NSPEEDZONES];
TinyGPS gps;
SoftwareSerial nss(3, 4);
boolean buttonPressed = false;
SoftwareSerial cell(7,8);  // We need to create a serial port on D2/D3 to talk to the GSM module
char mobilenumber[] = "+919901999868";  // Replace xxxxxxxx with the recipient's mobile number



void setup() {
  Serial.begin(9600);
  setupSpeedZones();
  blue = 12;
  red=11;
  pinMode(blue, OUTPUT);
  pinMode(red, OUTPUT);
  cell.begin(9600);
  delay(3500); // give the GSM module time to initialise, locate network etc.


  // Allow EM-406a to power up
  delay(3000);

  // Establish serial connection to EM-406a
  nss.begin(9600);
}



void setupSpeedZones() {



speedZones[0] = &SpeedZone(10);
speedZones[0]->setVertices(10, (Vertex[10]){
Vertex(12.938231,77.533291),
Vertex(12.937279,77.533835),
Vertex(12.936665,77.534077),
Vertex(12.93524,77.536153),
Vertex(12.933635,77.538924),
Vertex(12.934012,77.53902),
Vertex(12.935515,77.536367),
Vertex(12.936756,77.534332),
Vertex(12.937342,77.53412),
Vertex(12.938456,77.533546)});
 
speedZones[1] = &SpeedZone(2);
speedZones[1]->setVertices(6,(Vertex[6]){
Vertex(12.933763,77.539398),
Vertex(12.93242,77.541209),
Vertex(12.931058,77.543014),
Vertex(12.930901,77.542864),
Vertex(12.932271,77.541037),
Vertex(12.933512,77.539211)});
      
 
speedZones[2] = &SpeedZone(45);
speedZones[2]->setVertices(6, (Vertex[6]){
Vertex(12.934357,77.539017),
Vertex(12.936576,77.539626),
Vertex(12.937802,77.539793),
Vertex(12.937797,77.539951),
Vertex(12.93656,77.539865),
Vertex(12.934346,77.539208)});
      

speedZones[3] = &SpeedZone(40);
speedZones[3]->setVertices(4, (Vertex[4]){
Vertex(12.942973,77.538151),
Vertex(12.942994,77.539524),
Vertex(12.940986,77.539675),
Vertex(12.941044,77.538242)});
		

speedZones[4] = &SpeedZone(1);
speedZones[4]->setVertices(4, (Vertex[4]){
Vertex(12.935193,77.535496),
Vertex(12.933238,77.535635),
Vertex(12.933165,77.534283),
Vertex(12.935219,77.534155)});
      
      


  if (debugMode) {
    printSpeedZones();
  }

}

/*
 * This is the point-in-polygon algorithm adapted from
 * http://www.ecse.rpi.edu/Homepages/wrf/Research/Short_Notes/pnpoly.html
 */
boolean inSpeedZone(int speedZone, float lat, float lng) {
  SpeedZone *s = speedZones[speedZone];

  int i, j;
  boolean inside = false;
  for (i = 0, j = s->nVertices-1; i < s->nVertices; j = i++) {
    if ( ((s->vertices[i].lat > lat) != (s->vertices[j].lat > lat)) &&
         (lng < (s->vertices[j].lng - s->vertices[i].lng) * (lat - s->vertices[i].lat) / (s->vertices[j].lat - s->vertices[i].lat) + s->vertices[i].lng) )
       inside = !inside;
  }

  return inside;
}


boolean inSpeedZone(int speedZone) {
  float lat, lng;
  unsigned long  fix_age;

  // retrieves +/- lat/long in 100,000ths of a degree
  gps.f_get_position(&lat, &lng, &fix_age);

  return inSpeedZone(speedZone, lat, lng);
}
void loop() {
 if (readGPS()) {
    if (debugMode) {
      debug();
    }
    speeding = isSpeeding();
  }

  
  if (speeding ) {
    Serial.println("loop1");
    policeLights();
  } else {
    allOff();
  }

}

bool readGPS() {
  while (nss.available()) {
    if (gps.encode(nss.read())) {
      return true;
    }
  }
  return false;
}

  
int getSpeedLimit() {
  boolean isInSpeedZone;

  for(int i=0;i<NSPEEDZONES;i++) {
    isInSpeedZone = inSpeedZone(i);
    if (isInSpeedZone) {
      return speedZones[i]->speedLimit;
    }
   
     
  }
  return DEFAULT_SPEED_LIMIT;
}

boolean isSpeeding() {
  int speed = (int)(gps.f_speed_kmph() + 0.5);
  int speedLimit = getSpeedLimit();

  if (speed > speedLimit) {
    return true;
  }
  return false;
}

void policeLights() {
nss.end();
cell.begin(9600);
delay(3500);
digitalWrite(blue, HIGH);
digitalWrite(red, HIGH);
Serial.println("before delay");
cell.println("AT+CMGF=1"); // set SMS mode to text
cell.print("AT+CMGS=");  // now send message...
cell.write((byte)34);  // ASCII equivalent of "
cell.print(mobilenumber);
cell.write((byte)34);   // ASCII equivalent of "
cell.println();
delay(500); // give the module some thinking time
cell.print("hi bobby, the king of kings... :-)");   // our message to send
cell.write((byte)26); // ASCII equivalent of Ctrl-Z
cell.println();
delay(15000); // the SMS module needs time to return to OK status
Serial.println("after delay");
  cell.end();
nss.begin(9600);
}






void allOff() {
    digitalWrite(blue,LOW);
    digitalWrite(red, LOW);
    }

void printSpeedZones() {

  for(int i=0;i<NSPEEDZONES;i++) {
    SpeedZone *s = speedZones[i];
    Serial.println(s->speedLimit);
    for(int v=0;v<s->nVertices;v++) {
      Serial.print("(");
      Serial.print(s->vertices[v].lat,6);
      Serial.print(", ");
      Serial.print(s->vertices[v].lng,6);
      Serial.println(")");
    }
  }
}

void debug() {
  float lat, lng;
  unsigned long fix_age, time, date, speed, course;

  // retrieves +/- lat/long in 100000ths of a degree
  gps.f_get_position(&lat, &lng, &fix_age);

  Serial.println(getSpeedLimit());

  Serial.print("lat: ");
  Serial.print(lat,6);
  Serial.print("    lng: ");
  Serial.print(lng,6);
  Serial.print("    speed: ");
  Serial.println(gps.f_speed_kmph());
}

this is the output. As soon as the speed limit is crossed, gps data stops and gsm message is sent, and it keeps on coming, even though the current speed has gone below the speedlimit.

10

(12.938232, 77.533294)

(12.937279, 77.533836)

(12.936665, 77.534080)

(12.935240, 77.536155)

(12.933635, 77.538925)

(12.934013, 77.539016)

(12.935516, 77.536369)

(12.936757, 77.534332)

(12.937342, 77.534118)

(12.938456, 77.533546)

2

(12.933763, 77.539398)

(12.932420, 77.541206)

(12.931058, 77.543014)

(12.930901, 77.542861)

(12.932271, 77.541038)

(12.933512, 77.539207)

45

(12.934357, 77.539016)

(12.936576, 77.539627)

(12.937803, 77.539794)

(12.937797, 77.539947)

(12.936560, 77.539863)

(12.934347, 77.539207)

40

(12.942974, 77.538154)

(12.942995, 77.539520)

(12.940986, 77.539672)

(12.941044, 77.538238)

1

(12.935194, 77.535499)

(12.933238, 77.535636)

(12.933165, 77.534286)

(12.935219, 77.534156)

45

lat: 12.933341 lng: 77.534431 speed: -1.00

1

lat: 12.933341 lng: 77.534431 speed: 0.00

1

lat: 12.933341 lng: 77.534431 speed: 0.00

1

lat: 12.933341 lng: 77.534431 speed: 0.00

1

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933341 lng: 77.534431 speed: 0.00

2

lat: 12.933330 lng: 77.534439 speed: 0.00

2

lat: 12.933330 lng: 77.534439 speed: 2.76

loop1

before delay

after delay

loop1

before delay

after delay

loop1

before delay

after delay

loop1

before delay

after delay

loop1

before delay

after delay

loop1

As written, that code will kill the gps serial connection, then later start a new gps serial connection and call a read from the gps before it has time to update. Then, it will kill the gps serial connection, start a new connection later… etc. You would not receive any gps data because the gps updates about every second (1000 ms) but, you start a connection and request data a couple of ms later. Then, you kill the connection a few ms after that.

I’ve added debug printlns to your code and removed the kill/new cycle in policeLights. This is an excessive number of debugging statements , but it will let you see what is going on inside your program. Run it and see if you can figure out where it’s going wrong. If not, post the serial output and we can help you. I’ve left in the buttonPressed variable, though it is not altered in the code. You can add that logic back in to add that functionality.

I’ve also declared the functions near where the global variables are declared and put the functions themselves at the end. This makes the code a little cleaner looking. I To make it really organized, you should list the function declaration in the order they are used and follow that same order when listing the functions themselves at the end. I’ll leave that task to you. I just copied/pasted to get them out of the way.

    #include <SoftwareSerial.h>
    #include <TinyGPS.h>

    #define NUM_OFF 2
    #define DELAY 50
    #define DEFAULT_SPEED_LIMIT 50
    #define NSPEEDZONES 5

    boolean debugMode = true;
    boolean speeding = false;
    int blue;
    int red;

class Vertex {
    public:
      Vertex(float llat, float llng) {
        lat = llat;
        lng = llng;
      }
      float lat;
      float lng;
    };

class SpeedZone {
    public:
      SpeedZone(int s) {
        speedLimit = s;
      }
      void setVertices(int n, Vertex *v) {
        nVertices = n;
        vertices = v;
      }
      int nVertices;
      Vertex *vertices;
      int speedLimit;
    };

    SpeedZone *speedZones[NSPEEDZONES];
    TinyGPS gps;
    SoftwareSerial nss(3, 4);
    boolean buttonPressed = false;
    SoftwareSerial cell(7,8);  // We need to create a serial port on D2/D3 to talk to the GSM module
    char mobilenumber[] = "XXXXXXXXXXX";  // Replace xxxxxxxx with the recipient's mobile number
    
    //DECLARE FUNCTIONS
    void setupSpeedZones();
    boolean inSpeedZone(int speedZone, float lat, float lng);
    boolean inSpeedZone(int speedZone);
    boolean readGPS();
    boolean isSpeeding();
    void policeLights();
    void allOff();
    void debug();
    
    void setup() {
      Serial.begin(9600);
      setupSpeedZones();
      blue = 12;
      red=11;
      pinMode(blue, OUTPUT);
      pinMode(red, OUTPUT);
      cell.begin(9600);
      delay(3500); // give the GSM module time to initialise, locate network etc.

      // Allow EM-406a to power up
      delay(3000);

      // Establish serial connection to EM-406a
      nss.begin(9600);
      Serial.println("EXIT SETUP");
//      nss.listen();
    }//END SETUP
    
    void loop() {
      Serial.println("START LOOP");
     if (readGPS())
     {
       Serial.println("INSIDE LOOP FIRST IF, BEFORE DEBUG"); 
       if (debugMode) 
       {
          Serial.println("INSIDE LOOP SECOND IF, BEFORE DEBUG");
          debug();
       }
       Serial.println("INSIDE LOOP FIRST IF, AFTER DEBUG"); 
        speeding = isSpeeding();
      }//END FIRST IF
     
      if (speeding )
      {
        Serial.println("INSIDE LOOP THRID IF, BEFORE POLICELIGHTS");
        policeLights();
      }else //END SECOND IF
      {
         Serial.println("INSIDE LOOP THIRD IF, BEFORE ALLOFF"); 
         allOff();
      }
       Serial.println("END OF LOOP"); 
    }//END LOOP




//START INLINE FUNCTIONS

    boolean readGPS() {
      Serial.println("START READGPS"); 
      
      while (nss.available()) {
        if (gps.encode(nss.read())) {
          Serial.println("RETURNING TRUE");
          return true;
        }
      }
      Serial.println("RETURNING FALSE");
      return false;
    }//END READGPS

     
    int getSpeedLimit() {
      Serial.println("START GETSPEEDLIMIT");
      boolean isInSpeedZone;

      for(int i=0;i<NSPEEDZONES;i++) {
        isInSpeedZone = inSpeedZone(i);
        if (isInSpeedZone) {
          Serial.print("RETURNING SPEEDZONE, END GETSPEEDLIMIT");
          return speedZones[i]->speedLimit;
        }
       
         
      }
      Serial.println("RETURNING DEFAULT SPEEDZONE, END GETSPEEDLIMIT");
      return DEFAULT_SPEED_LIMIT;
    }//ENDGETSPEEDLIMIT

    boolean isSpeeding() {
      Serial.println("START ISSPEEDING");
      int speed = (int)(gps.f_speed_kmph() + 0.5);
      int speedLimit = getSpeedLimit();

      if (speed > speedLimit) 
      {  
        Serial.println("INSIDE ISSPEEDING IF, RETURNING SPEEDING IS TRUE");
        return true;
      }
      Serial.println("END ISSPEEDING, RETURNING SPEEDING IS FALSE");
      return false;
    }//END SPEEDING

    void policeLights() {
//    cell.listen();
    Serial.println("START POLICELIGHTS");
    digitalWrite(blue, HIGH);
    digitalWrite(red, HIGH);
    Serial.println("SENDING AT COMMANDS");
    cell.println("AT+CMGF=1"); // set SMS mode to text
    cell.print("AT+CMGS=");  // now send message...
    cell.write((byte)34);  // ASCII equivalent of "
    cell.print(mobilenumber);
    cell.write((byte)34);   // ASCII equivalent of "
    cell.println();
    delay(500); // give the module some thinking time
    cell.print("hi bobby, the king of kings... :-)");   // our message to send
    cell.write((byte)26); // ASCII equivalent of Ctrl-Z
    cell.println();
//    nss.listen();
    delay(15000); // the SMS module needs time to return to OK status
    Serial.println("AFTER 15 SECOND DELAY, END POLICELIGHTS");
    }//END POLICELIGHTS


    void allOff() {
      Serial.println("START ALLOFF"); 
      digitalWrite(blue,LOW);
      digitalWrite(red, LOW);
      Serial.println("END ALLOFF");
        }//END ALLOFF

    void printSpeedZones() {
      Serial.println("START PRINTSPEEDZONES");
      for(int i=0;i<NSPEEDZONES;i++) {
        SpeedZone *s = speedZones[i];
        Serial.println(s->speedLimit);
        for(int v=0;v<s->nVertices;v++) {
          Serial.print("(");
          Serial.print(s->vertices[v].lat,6);
          Serial.print(", ");
          Serial.print(s->vertices[v].lng,6);
          Serial.println(")");
        }
      }
      Serial.println("END PRINTSPEEDZONES");
    }//END PRINTSPEEDZONES

    void debug() {
      Serial.println("START DEBUG");
      float lat, lng;
      unsigned long fix_age, time, date, speed, course;

      // retrieves +/- lat/long in 100000ths of a degree
      gps.f_get_position(&lat, &lng, &fix_age);

      Serial.println(getSpeedLimit());

      Serial.print("lat: ");
      Serial.print(lat,6);
      Serial.print("    lng: ");
      Serial.print(lng,6);
      Serial.print("    speed: ");
      Serial.println(gps.f_speed_kmph());
      Serial.println("END DEBUG");
    }//END DEBUG
    
    void setupSpeedZones() {
      Serial.println("START SETUPSPEEDZONES");


    speedZones[0] = &SpeedZone(10);
    speedZones[0]->setVertices(10, (Vertex[10]){
    Vertex(12.938231,77.533291),
    Vertex(12.937279,77.533835),
    Vertex(12.936665,77.534077),
    Vertex(12.93524,77.536153),
    Vertex(12.933635,77.538924),
    Vertex(12.934012,77.53902),
    Vertex(12.935515,77.536367),
    Vertex(12.936756,77.534332),
    Vertex(12.937342,77.53412),
    Vertex(12.938456,77.533546)});
     
    speedZones[1] = &SpeedZone(2);
    speedZones[1]->setVertices(6,(Vertex[6]){
    Vertex(12.933763,77.539398),
    Vertex(12.93242,77.541209),
    Vertex(12.931058,77.543014),
    Vertex(12.930901,77.542864),
    Vertex(12.932271,77.541037),
    Vertex(12.933512,77.539211)});
         
     
    speedZones[2] = &SpeedZone(45);
    speedZones[2]->setVertices(6, (Vertex[6]){
    Vertex(12.934357,77.539017),
    Vertex(12.936576,77.539626),
    Vertex(12.937802,77.539793),
    Vertex(12.937797,77.539951),
    Vertex(12.93656,77.539865),
    Vertex(12.934346,77.539208)});
         

    speedZones[3] = &SpeedZone(40);
    speedZones[3]->setVertices(4, (Vertex[4]){
    Vertex(12.942973,77.538151),
    Vertex(12.942994,77.539524),
    Vertex(12.940986,77.539675),
    Vertex(12.941044,77.538242)});
          

    speedZones[4] = &SpeedZone(1);
    speedZones[4]->setVertices(4, (Vertex[4]){
    Vertex(12.935193,77.535496),
    Vertex(12.933238,77.535635),
    Vertex(12.933165,77.534283),
    Vertex(12.935219,77.534155)});
         
         


      if (debugMode) {
        Serial.println("INSIDE SETUPSPEEDZONE IF, BEFORE PRINTSPEEDZONES");
        printSpeedZones();
      }
      Serial.println("EXIT SETUPSPEEDZONES");
    }//END SETUPSPEEDZONES
    
    /*
     * This is the point-in-polygon algorithm adapted from
     * http://www.ecse.rpi.edu/Homepages/wrf/Research/Short_Notes/pnpoly.html
     */
    boolean inSpeedZone(int speedZone, float lat, float lng) {
      Serial.println("START INSPEEDZONE(LAT/LONG)");
      SpeedZone *s = speedZones[speedZone];

      int i, j;
      boolean inside = false;
      for (i = 0, j = s->nVertices-1; i < s->nVertices; j = i++) {
        if ( ((s->vertices[i].lat > lat) != (s->vertices[j].lat > lat)) &&
             (lng < (s->vertices[j].lng - s->vertices[i].lng) * (lat - s->vertices[i].lat) / (s->vertices[j].lat - s->vertices[i].lat) + s->vertices[i].lng) )
        {
          Serial.println("INSIDE IF, SETTING SPEEDZONE TRUE");
          inside = !inside;
        }//END IF
      }//END FOR LOOP
      Serial.println("END INSPEEDZONE(LAT/LONG)");
      return inside;
    }//END INSPEEDZONE


    boolean inSpeedZone(int speedZone) {
      Serial.println("START INSPEEDZONE(INT)");
      float lat, lng;
      unsigned long  fix_age;

      // retrieves +/- lat/long in 100,000ths of a degree
      gps.f_get_position(&lat, &lng, &fix_age);
      Serial.println("END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)");
      return inSpeedZone(speedZone, lat, lng);
      
     }//END INSPEEZONE

I’ve added a couple of listen() function calls but commented them out. I don’t think you need them, but you can uncomment them to ensure you are listening to the serial connection you want.

WethaGuy:
As written, that code will kill the gps serial connection, then later start a new gps serial connection and call a read from the gps before it has time to update. Then, it will kill the gps serial connection, start a new connection later… etc. You would not receive any gps data because the gps updates about every second (1000 ms) but, you start a connection and request data a couple of ms later. Then, you kill the connection a few ms after that.

I’ve added debug printlns to your code and removed the kill/new cycle in policeLights. This is an excessive number of debugging statements , but it will let you see what is going on inside your program. Run it and see if you can figure out where it’s going wrong. If not, post the serial output and we can help you. I’ve left in the buttonPressed variable, though it is not altered in the code. You can add that logic back in to add that functionality.

I’ve also declared the functions near where the global variables are declared and put the functions themselves at the end. This makes the code a little cleaner looking. I To make it really organized, you should list the function declaration in the order they are used and follow that same order when listing the functions themselves at the end. I’ll leave that task to you. I just copied/pasted to get them out of the way.

    #include <SoftwareSerial.h>
#include <TinyGPS.h>

#define NUM_OFF 2
#define DELAY 50
#define DEFAULT_SPEED_LIMIT 50
#define NSPEEDZONES 5

boolean debugMode = true;
boolean speeding = false;
int blue;
int red;

class Vertex {
public:
Vertex(float llat, float llng) {
lat = llat;
lng = llng;
}
float lat;
float lng;
};

class SpeedZone {
public:
SpeedZone(int s) {
speedLimit = s;
}
void setVertices(int n, Vertex *v) {
nVertices = n;
vertices = v;
}
int nVertices;
Vertex *vertices;
int speedLimit;
};

SpeedZone *speedZones[NSPEEDZONES];
TinyGPS gps;
SoftwareSerial nss(3, 4);
boolean buttonPressed = false;
SoftwareSerial cell(7,8);  // We need to create a serial port on D2/D3 to talk to the GSM module
char mobilenumber[] = "XXXXXXXXXXX";  // Replace xxxxxxxx with the recipient's mobile number

//DECLARE FUNCTIONS
void setupSpeedZones();
boolean inSpeedZone(int speedZone, float lat, float lng);
boolean inSpeedZone(int speedZone);
boolean readGPS();
boolean isSpeeding();
void policeLights();
void allOff();
void debug();

void setup() {
  Serial.begin(9600);
  setupSpeedZones();
  blue = 12;
  red=11;
  pinMode(blue, OUTPUT);
  pinMode(red, OUTPUT);
  cell.begin(9600);
  delay(3500); // give the GSM module time to initialise, locate network etc.

  // Allow EM-406a to power up
  delay(3000);

  // Establish serial connection to EM-406a
  nss.begin(9600);
  Serial.println("EXIT SETUP");

// nss.listen();
}//END SETUP

void loop() {
  Serial.println("START LOOP");
 if (readGPS())
 {
   Serial.println("INSIDE LOOP FIRST IF, BEFORE DEBUG"); 
   if (debugMode) 
   {
      Serial.println("INSIDE LOOP SECOND IF, BEFORE DEBUG");
      debug();
   }
   Serial.println("INSIDE LOOP FIRST IF, AFTER DEBUG"); 
    speeding = isSpeeding();
  }//END FIRST IF
 
  if (speeding )
  {
    Serial.println("INSIDE LOOP THRID IF, BEFORE POLICELIGHTS");
    policeLights();
  }else //END SECOND IF
  {
     Serial.println("INSIDE LOOP THIRD IF, BEFORE ALLOFF"); 
     allOff();
  }
   Serial.println("END OF LOOP"); 
}//END LOOP

//START INLINE FUNCTIONS

boolean readGPS() {
  Serial.println("START READGPS"); 
  
  while (nss.available()) {
    if (gps.encode(nss.read())) {
      Serial.println("RETURNING TRUE");
      return true;
    }
  }
  Serial.println("RETURNING FALSE");
  return false;
}//END READGPS

 
int getSpeedLimit() {
  Serial.println("START GETSPEEDLIMIT");
  boolean isInSpeedZone;

  for(int i=0;i<NSPEEDZONES;i++) {
    isInSpeedZone = inSpeedZone(i);
    if (isInSpeedZone) {
      Serial.print("RETURNING SPEEDZONE, END GETSPEEDLIMIT");
      return speedZones[i]->speedLimit;
    }
   
     
  }
  Serial.println("RETURNING DEFAULT SPEEDZONE, END GETSPEEDLIMIT");
  return DEFAULT_SPEED_LIMIT;
}//ENDGETSPEEDLIMIT

boolean isSpeeding() {
  Serial.println("START ISSPEEDING");
  int speed = (int)(gps.f_speed_kmph() + 0.5);
  int speedLimit = getSpeedLimit();

  if (speed > speedLimit) 
  {  
    Serial.println("INSIDE ISSPEEDING IF, RETURNING SPEEDING IS TRUE");
    return true;
  }
  Serial.println("END ISSPEEDING, RETURNING SPEEDING IS FALSE");
  return false;
}//END SPEEDING

void policeLights() {

// cell.listen();
Serial.println(“START POLICELIGHTS”);
digitalWrite(blue, HIGH);
digitalWrite(red, HIGH);
Serial.println(“SENDING AT COMMANDS”);
cell.println(“AT+CMGF=1”); // set SMS mode to text
cell.print(“AT+CMGS=”); // now send message…
cell.write((byte)34); // ASCII equivalent of "
cell.print(mobilenumber);
cell.write((byte)34); // ASCII equivalent of "
cell.println();
delay(500); // give the module some thinking time
cell.print(“hi bobby, the king of kings… :-)”); // our message to send
cell.write((byte)26); // ASCII equivalent of Ctrl-Z
cell.println();
// nss.listen();
delay(15000); // the SMS module needs time to return to OK status
Serial.println(“AFTER 15 SECOND DELAY, END POLICELIGHTS”);
}//END POLICELIGHTS

void allOff() {
  Serial.println("START ALLOFF"); 
  digitalWrite(blue,LOW);
  digitalWrite(red, LOW);
  Serial.println("END ALLOFF");
    }//END ALLOFF

void printSpeedZones() {
  Serial.println("START PRINTSPEEDZONES");
  for(int i=0;i<NSPEEDZONES;i++) {
    SpeedZone *s = speedZones[i];
    Serial.println(s->speedLimit);
    for(int v=0;v<s->nVertices;v++) {
      Serial.print("(");
      Serial.print(s->vertices[v].lat,6);
      Serial.print(", ");
      Serial.print(s->vertices[v].lng,6);
      Serial.println(")");
    }
  }
  Serial.println("END PRINTSPEEDZONES");
}//END PRINTSPEEDZONES

void debug() {
  Serial.println("START DEBUG");
  float lat, lng;
  unsigned long fix_age, time, date, speed, course;

  // retrieves +/- lat/long in 100000ths of a degree
  gps.f_get_position(&lat, &lng, &fix_age);

  Serial.println(getSpeedLimit());

  Serial.print("lat: ");
  Serial.print(lat,6);
  Serial.print("    lng: ");
  Serial.print(lng,6);
  Serial.print("    speed: ");
  Serial.println(gps.f_speed_kmph());
  Serial.println("END DEBUG");
}//END DEBUG

void setupSpeedZones() {
  Serial.println("START SETUPSPEEDZONES");


speedZones[0] = &SpeedZone(10);
speedZones[0]->setVertices(10, (Vertex[10]){
Vertex(12.938231,77.533291),
Vertex(12.937279,77.533835),
Vertex(12.936665,77.534077),
Vertex(12.93524,77.536153),
Vertex(12.933635,77.538924),
Vertex(12.934012,77.53902),
Vertex(12.935515,77.536367),
Vertex(12.936756,77.534332),
Vertex(12.937342,77.53412),
Vertex(12.938456,77.533546)});
 
speedZones[1] = &SpeedZone(2);
speedZones[1]->setVertices(6,(Vertex[6]){
Vertex(12.933763,77.539398),
Vertex(12.93242,77.541209),
Vertex(12.931058,77.543014),
Vertex(12.930901,77.542864),
Vertex(12.932271,77.541037),
Vertex(12.933512,77.539211)});
     
 
speedZones[2] = &SpeedZone(45);
speedZones[2]->setVertices(6, (Vertex[6]){
Vertex(12.934357,77.539017),
Vertex(12.936576,77.539626),
Vertex(12.937802,77.539793),
Vertex(12.937797,77.539951),
Vertex(12.93656,77.539865),
Vertex(12.934346,77.539208)});
     

speedZones[3] = &SpeedZone(40);
speedZones[3]->setVertices(4, (Vertex[4]){
Vertex(12.942973,77.538151),
Vertex(12.942994,77.539524),
Vertex(12.940986,77.539675),
Vertex(12.941044,77.538242)});
      

speedZones[4] = &SpeedZone(1);
speedZones[4]->setVertices(4, (Vertex[4]){
Vertex(12.935193,77.535496),
Vertex(12.933238,77.535635),
Vertex(12.933165,77.534283),
Vertex(12.935219,77.534155)});
     
     


  if (debugMode) {
    Serial.println("INSIDE SETUPSPEEDZONE IF, BEFORE PRINTSPEEDZONES");
    printSpeedZones();
  }
  Serial.println("EXIT SETUPSPEEDZONES");
}//END SETUPSPEEDZONES

/*
 * This is the point-in-polygon algorithm adapted from
 * http://www.ecse.rpi.edu/Homepages/wrf/Research/Short_Notes/pnpoly.html
 */
boolean inSpeedZone(int speedZone, float lat, float lng) {
  Serial.println("START INSPEEDZONE(LAT/LONG)");
  SpeedZone *s = speedZones[speedZone];

  int i, j;
  boolean inside = false;
  for (i = 0, j = s->nVertices-1; i < s->nVertices; j = i++) {
    if ( ((s->vertices[i].lat > lat) != (s->vertices[j].lat > lat)) &&
         (lng < (s->vertices[j].lng - s->vertices[i].lng) * (lat - s->vertices[i].lat) / (s->vertices[j].lat - s->vertices[i].lat) + s->vertices[i].lng) )
    {
      Serial.println("INSIDE IF, SETTING SPEEDZONE TRUE");
      inside = !inside;
    }//END IF
  }//END FOR LOOP
  Serial.println("END INSPEEDZONE(LAT/LONG)");
  return inside;
}//END INSPEEDZONE


boolean inSpeedZone(int speedZone) {
  Serial.println("START INSPEEDZONE(INT)");
  float lat, lng;
  unsigned long  fix_age;

  // retrieves +/- lat/long in 100,000ths of a degree
  gps.f_get_position(&lat, &lng, &fix_age);
  Serial.println("END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)");
  return inSpeedZone(speedZone, lat, lng);
  
 }//END INSPEEZONE



I've added a couple of listen() function calls but commented them out. I don't think you need them, but you can uncomment them to ensure you are listening to the serial connection you want.

This is the output I am getting. I think you can see that once the speeding condition is satisfied, gsm comes into action, and there after gps data is not read at all. The program keeps on sending messages.

START SETUPSPEEDZONES

INSIDE SETUPSPEEDZONE IF, BEFORE PRINTSPEEDZONES

START PRINTSPEEDZONES

-1

(12.938232, 77.533294)

(12.937279, 77.533836)

(12.936665, 77.534080)

(12.935240, 77.536155)

(12.933635, 77.538925)

(12.934013, 77.539016)

(12.935516, 77.536369)

(12.936757, 77.534332)

(12.937342, 77.534118)

(12.938456, 77.533546)

-1

(12.933763, 77.539398)

(12.932420, 77.541206)

(12.931058, 77.543014)

(12.930901, 77.542861)

(12.932271, 77.541038)

(12.933512, 77.539207)

-1

(12.934357, 77.539016)

(12.936576, 77.539627)

(12.937803, 77.539794)

(12.937797, 77.539947)

(12.936560, 77.539863)

(12.934347, 77.539207)

-1

(12.942974, 77.538154)

(12.942995, 77.539520)

(12.940986, 77.539672)

(12.941044, 77.538238)

-1

(12.935194, 77.535499)

(12.933238, 77.535636)

(12.933165, 77.534286)

(12.935219, 77.534156)

END PRINTSPEEDZONES

EXIT SETUPSPEEDZONES

EXIT SETUP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THIRD IF, BEFORE ALLOFF

START ALLOFF

END ALLOFF

END OF LOOP

START LOOP

START READGPS

RETURNING TRUE

INSIDE LOOP FIRST IF, BEFORE DEBUG

INSIDE LOOP SECOND IF, BEFORE DEBUG

START DEBUG

START GETSPEEDLIMIT

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

END INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

INSIDE IF, SETTING SPEEDZONE TRUE

INSIDE IF, SETTING SPEEDZONE TRUE

END INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

END INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

END INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

INSIDE IF, SETTING SPEEDZONE TRUE

END INSPEEDZONE(LAT/LONG)

RETURNING SPEEDZONE, END GETSPEEDLIMIT-1

lat: 12.933461 lng: 77.534500 speed: -1.00

END DEBUG

INSIDE LOOP FIRST IF, AFTER DEBUG

START ISSPEEDING

START GETSPEEDLIMIT

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

END INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(INT)

END INSPEEDZONE(INT), CALLING INSPEEDZONE(LAT/LONG)

START INSPEEDZONE(LAT/LONG)

INSIDE IF, SETTING SPEEDZONE TRUE

END INSPEEDZONE(LAT/LONG)

RETURNING SPEEDZONE, END GETSPEEDLIMITINSIDE ISSPEEDING IF, RETURNING SPEEDING IS TRUE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

AFTER 15 SECOND DELAY, END POLICELIGHTS

END OF LOOP

START LOOP

START READGPS

RETURNING FALSE

INSIDE LOOP THRID IF, BEFORE POLICELIGHTS

START POLICELIGHTS

SENDING AT COMMANDS

bobxcool:
… I think you can see that once the speeding condition is satisfied, gsm comes into action, and there after gps data is not read at all. …

Good troubleshooting. You’ve identified exactly where the problem is. The gsm must be continously talking with the arduino on the serial line and not letting it listen on other lines. This should be solved with uncommenting those 3 calls to listen(). You may have to move that one listen() call to after the 15 second delay, if the gsm module requires an ack from the serial connection after sending the message to remain in “OK” state. I’m not familiar with gsm, but if you can issue some kind of “wait” command to the gsm module, you wouldn’t need to listen() calll. Just talk to the gsm in policeLights(), then tell it to wait.

WethaGuy:

bobxcool:
… I think you can see that once the speeding condition is satisfied, gsm comes into action, and there after gps data is not read at all. …

Good troubleshooting. You’ve identified exactly where the problem is. The gsm must be continously talking with the arduino on the serial line and not letting it listen on other lines. This should be solved with uncommenting those 3 calls to listen(). You may have to move that one listen() call to after the 15 second delay, if the gsm module requires an ack from the serial connection after sending the message to remain in “OK” state. I’m not familiar with gsm, but if you can issue some kind of “wait” command to the gsm module, you wouldn’t need to listen() calll. Just talk to the gsm in policeLights(), then tell it to wait.

sir, this the output I posted was with listen commands you had mentioned , but I had un-commented them.

It could be interference with the gps receiving signals or electrical interference in your circuit. As I said, I’m not familiar with gsm but you can try this:

Comment out all the cell writes and prints except ```
cell.println(“AT+CMGF=1”); // set SMS mode to text


This should not cause the cell to go to high power or radiate any signal beyond what it is already doing (I'm totally guessing on this, check your datasheet). If this does not solve it, the problem is likely electrical interference in your circuit (grounds not connected, all using same power supply, brownout, inadequate rf shielding in the circuit, etc...). If everything works, then your gsm module is interfering with your gps and you need to move them further apart or wait until the gsm goes low power again.

WethaGuy:
It could be interference with the gps receiving signals or electrical interference in your circuit. As I said, I’m not familiar with gsm but you can try this:

Comment out all the cell writes and prints except ```
cell.println(“AT+CMGF=1”); // set SMS mode to text


This should not cause the cell to go to high power or radiate any signal beyond what it is already doing (I'm totally guessing on this, check your datasheet). If this does not solve it, the problem is likely electrical interference in your circuit (grounds not connected, all using same power supply, brownout, inadequate rf shielding in the circuit, etc...). If everything works, then your gsm module is interfering with your gps and you need to move them further apart or wait until the gsm goes low power again.

I removed all the print statements you suggested, but I am not getting the message. (as I have removed the print statements which are needed for a message to be sent) But without these statements (you suggested), the gps did not get stuck anywhere.

As you said, I think I need to add some commands to stop the gsm module temporarily. I will create another post in the forums for this.

Please note: I have used separate power supplies for all the components and also had common ground connected for all.