Programming my Arduino board w AVRISP mkII

Hi All…

I have an Arduino compatible board a friend of mine and I built but I’m having some issues programming it. Some of them work, others don’t. I’m using AVR Studio 5.0 with an AVRISP mkII. Initially, I can read the device ID and fuses, but when I attempt to modify the fuses or lock bits, I get a verification error. After some attempts, I can’t even read the device ID any more.

I’m a bit confused as to why I can initially read the fuses and lock bits, and the device ID, but then I get to the point where I an not even get the device ID. The MPU is an ATmega1284P with a 16 MHz crystal.

The fuses I am setting are:

BODLEVEL: 2V7

OCDEN: NOT CHECKED

JTAGEN: NOT CHECKED

SPIEN: CHECKED

WDTON: NOT CHECKED

EESAVE: NOT CHECKED

BOOTSZ: 1024_FC00

BOOTRST: CHECKED

CKDIV8: NOT CHECKED

CKOUT: NOT CHECKED

SUT_CKSEL: EXTXOSC_8MHZ_XX_16KCK_65MS

EXTENDED: 0XFD

HIGH: 0XDC

LOW: 0XFF

Any suggestions are appreciated, thanks.

also, try avrfreaks.net forum

stevech:
also, try avrfreaks.net forum

I did, thanks, no luck so far there either.