I am looking to combine a Load sensor, Reed Switch, Battery, USB, Bluetooth.
I want the device to record load and #reed actuation associated with time. The output should be Load/Time and #Reed/Time and will be stored on USB or transmitted via Bluetooth.
Please help! :?
Perhaps a datalogger like …
https://www.sparkfun.com/products/10216
The Logomatic v2 uses a USB mass storage stack to appear under any operating system as a flash drive. Logs are created in FAT16 format on the micro-SD media and can be downloaded quickly over a USB connection by dragging and dropping the text files from the device. The microSD card can also be removed and inserted into a card reader to download the logs.
Board comes with a JST connector to be powered from our line-up of LiPo batteries or other power sources up to 7.5VDC. If you choose to use LiPo batteries, the Logomatic v2 has a built-in charger to charge batteries off USB.
The Logomatic v2 ships with basic serial text and analog logging.
Sent a P/M, also this is for someone to build! Thanks