I’ve been fighting gdb and open_ocd server all day and NOW –
All of a sudden I can’t write to flash after an erase.
flash erase 0 0 7
flash write 0 main.bin 0
flash program error
wrote file main.bin to flash bank 0 at offset 0x00000000
I just ran over 4K in program size but it looks like bank 0 is covered to 262K (lpc2103)
flash banks
#0: lpc2000 at 0x00000000, size 0x00040000, buswidth 0, chipwidth 0
#1: cfi at 0x80000000, size 0x00400000, buswidth 2, chipwidth 2
I also discovered this:
flash info 0
#1: lpc2000 at 0x00000000, size 0x00040000, buswidth 0, chipwidth 0
#0: 0x00000000 (0x2000kB) not erased, protected
#1: 0x00002000 (0x2000kB) erased, protected
#2: 0x00004000 (0x2000kB) erased, protected
#3: 0x00006000 (0x2000kB) erased, protected
#4: 0x00008000 (0x2000kB) erased, protected
#5: 0x0000a000 (0x2000kB) erased, protected
#6: 0x0000c000 (0x2000kB) erased, protected
#7: 0x0000e000 (0x2000kB) erased, protected
#8: 0x00010000 (0x10000kB) not erased, protected
#9: 0x00020000 (0x10000kB) not erased, protected
#10: 0x00030000 (0x2000kB) not erased, protected
#11: 0x00032000 (0x2000kB) not erased, protected
#12: 0x00034000 (0x2000kB) not erased, protected
#13: 0x00036000 (0x2000kB) not erased, protected
#14: 0x00038000 (0x2000kB) not erased, protected
#15: 0x0003a000 (0x2000kB) not erased, protected
#16: 0x0003c000 (0x2000kB) not erased, protected
#17: 0x0003e000 (0x2000kB) not erased, protected
Did the bank somehow get protected and is no longer usable?
I don’t know how to interpret the above information versus the Philips manual regarding sectors, so if anyone has a clue, let me know.
Any help will be much appreciated. Thanks.