Hello,
I am trying to get Example1_config_BPM_Mode1 from the from the SparkFun_Bio_Sensor_Library to work with a Arduino Nano 33 BLE sense with Nordic nRF52840 architecture. I am not using the Qwicc wiring, I have used a solder and checked and rechecked all my joints. When I run the example, it compiles, and gives no errors at any point, stating that the sensor is configured and connected, but outputs 0 for every metric. The red LED is also not running. Is this architecture not supported, if so, would I need to port the library to fit the nRF52840 architecture in order to make this hardware work?
Thank you in advance for your help.